infrastructure for a connected world
|
|
|
|
Partner Ecosystem |
Design Tools |
Literature Library |
Download Center |
Contact Us |
Training |
---|---|---|---|---|---|
Environmental extremes are not the only factors that create harsh environments. Indoor harsh conditions abound throughout plant and processing facilities, including high vibration, chemical vapors, galvanic corrosion and radiation that can also result in significant equipment wear-and-tear. In industrial applications, these are all variables that can interrupt production, cause downtime, and create safety hazards.
Click for more detailsReal-time access to patient related data and systems through high performance networks helps reduce medical errors and improve patient experience. Ultimately organizations will be able to deliver better care and services by improving the agility, flexibility, and integration of clinical and business operations.
Click for more detailsPanduit is committed to delivering innovative end-to-end solutions for electrical and networking installations that exceed industry demands. Our comprehensive range of products and installation tools meet the daily challenges of our Contractor Partners head on, and surpass their expectations in the most demanding applications and environments. This consistent performance assures our partners their ability to provide solutions to their customers’ toughest business challenges.
Click for more detailsThis brochure will walk you through the labeling requirements of the standard and introduce you to identification solutions specifically designed to comply with TIA/EIA-606-A.
Click for more detailsThe performance and reliability of networks within the Data Center are vital to the operation of today’s Enterprise. As the performance requirements of these networks have advanced to keep up with the data and virtualization explosion, the specifications on the constituent components have also become more demanding. For high-speed optical networks using laser-optimized multimode fiber (MMF) operating at 10 Gb/s today and 40 and 100 Gb/s in the near future, it is more critical than ever for network operators and designers to have an accurate knowledge of the performance specifications of the active and passive fiber optic components used to make up the network.
Click for more detailsIn recent years, virtualization, consolidation and the continuous treadmill of refresh cycles have dramatically changed the operation of data centers. Typically, a tremendous amount of planning goes into the network and application framework of an IT system without much regard being paid to the physical infrastructure. Part of the problem is that many do not have a clear understanding of what is included in the physical infrastructure and how critical it is to the functioning of an IT system. Panduit Advisory Services works with you to: improve performance, availability, scalability, and management of applications; mitigate risks related to convergence, security, safety, and compliance; reduce operating and energy costs; increase ROI relating to physical infrastructure systems; and support sustainability efforts. To learn more about our offerings, contact us at AdvisoryServices@panduit.com
Click for more detailsAs you plan and design your data center, you have the opportunity to include important infrastructure elements such as cable pathways, grounding and bonding, and identification, that if not adopted could have a significant impact on the operational efficiency and network reliability of your data center.
Click for more detailsPanduit and Cisco have created a data center solution that integrates the physical infrastructure systems needed in an optimized data center deployment. Panduit Pre-Configured Physical Infrastructures arrive at partner or end user sites ready to be deployed, reducing the time required for planning, designing, procurement, and installation, as well as the cost of operations.
Click for more detailsPanduit offers a comprehensive approach to the physical layer. The Unified Physical Infrastructure approach enables organizations to simplify their IT and network infrastructure while improving accessibility and increasing operational efficiencies.
Click for more detailsAudio/video systems are becoming more integrated with connectivity installations causing installers and contractors to look for a source that will best supply what is needed in the field. Panduit Audio/Video products are a comprehensive offering to fit the customers’ needs.
Click for more detailsEnable the continual creation of products and solutions that use energy efficiently, reduce resource consumption, and minimize your ecological footprint.
Click for more detailsDesign flexibility, verified optical performance and signal integrity far beyond the requirements for 10/40/100 Gb Ethernet, and 8 and 16 Gb Fibre with Signature Core™ Fiber Optic Cabling System.
Click for more detailsQuickNet™ Copper Cabling Systems for Deployment for High-Density Data Center Applications
Click for more detailsTo meet the demands and challenges facing government today, the deployment of e-Government solutions requires significant IT and infrastructure modernization that increases bandwidth for applications, expands access, and enhances availability. This increased reliance on technology makes it critical for government to invest in solutions that facilitate increased business agility, interoperability, and network security.
Click for more detailsPanduit supports the needs of small data centers with SmartZone™ Rack Energy Kits, a DCIM solution specifically designed to provide cost-effective power and environmental monitoring for small data center environments with 30 or fewer racks and cabin
Click for more detailsPanduit offers end-to-end copper cabling systems including patch cords, connectivity, and cable with best-in-class headroom warranties. Panduit's horizontal unshielded and shielded cable in Category 7A, 7, 6A, 6, and 5e performance levels exceed all applicable ANSI/TIA and ISO standards
Click for more detailsAchieving workplace safety throughout the physical infrastructure. Awareness of workplace safety and regulations,identification of safety hazards,procedures for bringing equipment to a zero energy state,training,safety devices and equipment.
Click for more detailsAs the world increasingly relies on clean, renewable energy sources, solar power has proven to be a smart choice for the future. Recent advances in panel design and manufacturing have significantly reduced costs and increased power output, helping solar producers take meaningful steps toward cost parity with conventional power generation.
Click for more detailsSolutions that address customer challenges while meeting and exceeding industry standards for performance, durability, and safety.
Click for more detailsClean and reliable power is key to data center performance and uptime.Panduit provides solutions for all of the critical connections from the utility transformer through the network equipment to protect your data center investment.
Click for more detailsPanduit's Wyr-Grid Overhead Cable Tray Routing System contributes to effective real estate usage and network performance. It provides speed of deployment, structural integrity, cable protection, and ease of use.
Click for more detailsPanduit Unified Physical Infrastructure based solutions help improve operational efficiencies, reduce unplanned downtime, and increase service and network security levels to fully address the demands of e-Government.
Click for more detailsThe Panduit ® Signature Core™ Fiber Optic Cabling System integrates ultra high performance laser-optimized, modal and dispersion compensated multimode fiber with low loss MTP* and single fiber connectivity solutions.
Click for more detailsThe Panduit Unified Physical Infrastructure Approach to Data, Power, Communication, Security and Control Systems from Panduit
Click for more detailsStructuredGround Kits for Data Center Cabinet Grounding complies with the “Telecommunications Infrastructure Standard for Data Centers” as described in TIA-942
Click for more detailsPanduit's switch, server, and storage equipment cabinet solutions significantly reduce total cost of ownership by increasing network availability, mitigating risk, and minimizing power consumption.
Click for more detailsAchieve Panel Space Optimization with PANELMAX ™ DIN Rail Wiring Duct.
Click for more detailsPanduit is always looking for talented, motivated people who have the skills needed to provide solutions to our customers. We value team players who can help us build a better Panduit and continually deliver value to our global customers. But more than that, at Panduit, you can make an impact. Our unique culture fosters an environment where great things can be accomplished through collaboration, problem solving and creativity. In return for your talents, we offer a wide variety of programs, services and resources to employees to improve their skills, grow in their career, and meet their commitments to both their personal lives and their jobs.
Click for more detailsMaximize space utilization to reduce capital expenditures and operational costs while maintaining network reliability and availability.
Click for more detailsPanduit provides a comprehensive line of wireless access point enclosures for indoor, industrial, and outdoor wireless LAN applications. The complete line of PanZone Wireless Access Point Enclosures accommodates a full range of wireless access points from industry leading manufacturers including Cisco Systems, Hewlett-Packard, Foundry Networks, and Enterasys Networks.
Click for more detailsBased on an understanding of today’s vital business and technology challenges and how they impact data centers, Panduit has created best-in-class physical infrastructure solutions for HSDT. Panduit provides the broadest offering of end-to-end HSDT solutions supporting all data center architectures. Designed for high-density/high-speed applications, Panduit HSDT solutions are backed by comprehensive research and development programs to ensure high network performance, systems reliability, energy efficiencies, and seamless integration.
Click for more detailsEquipment reliability and uptime are necessary for success in manufacturing environments, power generation facilities,and remote locations. From large panels in wind turbines that control generation parameters to robotic manufacturing equipment, panels are everywhere, and at an increasing rate, are network enabled requiring reliable connections.
Click for more detailsPanduit's Physical Infrastrucutre Manager Software Platform is a data center infrastructure management (DCIM) solution that provides accurate, automated, and centralized physical infrastructure visibility to help network stakeholders achieve service-oriented goals. These tools, dashboards, and reports enable you to make informed decisions to meet the demanding needs around capacity planning, remote management, and end-to-end service level agreements. This means that real-time information about connectivity, IT assets, power usage, thermal and environmental conditions, and space is now at your fingertips to provide complete data center infrastructure management.
Click for more detailsPanduit's Wyr-Grid® Overhead Cable Tray Routing System contributes to effective real estate usage and network performance. It provides speed of deployment, structural integrity, cable protection, and ease of use.
Click for more detailsReliable and flexible industrial networks are critical for maintaining productivity. Requirements range from the ability to trace production lot quality, to improving factory preventive maintenance schedules, to identification of constraints that decrease production. Protecting these networks from varying environmental conditions such as dusty and dirty to wet and corrosive on the production floor, is of vital importance.
Click for more details