building a smarter, unified business foundation

Fresh Insight

We look at things differently: from the bottom up. Often overlooked and underappreciated, the physical infrastructure has become more critical as networks converge, higher-powered computing equipment is developed, and business needs increase the demand for data…NOW!

We call this section Fresh Insight, because we want to share this unique perspective by allowing readers to Research, Learn, and Collaborate.  We believe these actions empower our clients to optimize their physical infrastructure to transform the way they do business.
 
Our door is always open. We invite you to share your questions, thoughts, and comments with us to improve Fresh Insight or, if you would like to suggest physical infrastructure topics for discussion, contact us at AdvisoryServices@panduit.com.

Featured Case Studies
 
image Hertz Corporation Case Study

Hertz Corporation needed a solution that would accommodate the essential requirements associated with establishing future-proof data centers as well as one that would help the company run its centers as efficiently as possible for complete optimization. In conjunction with this solution, Hertz needed a solutions provider that understood their commitment to customer service levels, quality, and reliability and could address their ultimate goals by accurately assessing their needs. Reliability and high availability are critical to Hertz’s worldwide operations, and the upgrade could only occur without interruption or delays. Read more…

Physical Infrastructure Design
 
 
 
More Case Studies
 
Reduced Energy Savings by 33%

Moving to a High-Performance Network with Stringent Security Protocols

Too Many "Hops" Spoil the Brew: Increasing Network Agility

Even if Lightning Doesn't Strike, You Need to be Grounded and Bonded

Twelve-Year-Old Fiber Was Holding Up a Nine-Figure Contract

Turning Office Space Into a Micro Data Center is a Snap

Featured White Papers
 
image
Physical Infrastructure Optimization: A Foundation for Growth.

According to Gartner, the rise in big data is one of the forces that will change IT. The proliferation of data is accelerating, and most IT departments are not prepared to handle the demands of managing and storing so much data. At the same time, corporate data centers
are ill-equipped to handle the flood, driving the need to consolidate and optimize the physical infrastructure. Read more...
Physical Infrastructure Optimization
image
A Critical Factor In Cloud Deployment

As companies begin to pilot cloud projects or deploy it in earnest, data center managers are discovering that migrating the data center to the cloud is not as simple as they had imagined. The cloud does reduce to some degree the amount of computing hardware a company needs for its data center. But many fail to consider that the cloud requires a robust physical infrastructure to maximize the expected benefits. Many executives are discovering too late that they did not focus enough on physical infrastructure design prior to the move to the cloud. This can jeopardize cloud deployments before they begin. Read more...
Virtualization
 

Featured Articles
 
image

High Tech Getting Too Hot?.

Proper airflow and thermal management are the most critical aspects of designing and operating your data center, ensuring uptime of applications, consistent IT equipment performance and efficient operations. In the past, data center managers would over supply a room with cold air to address small hot spots and perceived requirements for cooling the data center. Typical rack densities averaged 3 – 5 kW, thus the cooling requirements were moderate. Very few data center managers were pushing the envelope on operational efficiencies. They were smoothing over the imperfections. Read more...

Thermal Management Solutions
image

Reference Architecture: The Building Blocks of an Agile, Flexible, Scalable and Sustainable Foundation.

Many IT professionals believe that they need to start from scratch when designing their IT infrastructure because their business needs are unique and require specific strategies for a successful implementation. However, having a reference architecture in place simplifies decision making because it provides an initial blueprint that allows you to quickly develop multiple reference designs from the same architecture based on your business needs. With a solid reference architecture, you have the ability to modify the design for your business requirements, and understand how next generation technologies will advance your data center or enterprise to support future needs. Read more...

 

Design Services
image

Don't Get Blown Away By The Cloud: 5 Tips to Optimize Your Physical Infrastructure for Virtualization.

Proper airflow and thermal management are the most critical aspects of designing and operating your data center, ensuring uptime of applications, consistent IT equipment performance and efficient operations. In the past, data center managers would over supply a room with cold air to address small hot spots and perceived requirements for cooling the data center. Typical rack densities averaged 3 – 5 kW, thus the cooling requirements were moderate. Very few data center managers were pushing the envelope on operational efficiencies. They were smoothing over the imperfections. Read more...

Thermal Management Solutions
image

Common Sense: Solution to Make Your Data Center Energy Efficient

Energy efficiency is a life style. It’s also common sense. In a data center, the name of the game is efficiency and how many compute operations you can get for a given amount of power. You can change the numerator: Get more compute for your energy dollars or you can change the denominator
(reduce your power usage), but the fi rst step is to assess all the systems in order to improve your utilization and efficiency. Read more...

Energy Efficiency
image

Breath of Fresh Air: How ASHRAE’s 2011 Thermal Guidelines Can Help You Increase Efficiency and Save Money.

It seems strange that a data center would have trouble with overheating when around the globe many countries have cold air a majority of the year. A recent ASHRAE white paper demonstrates how in the Chicago area, the dry bulb temperatures are below 20°C (68°F) for roughly 5,000 to 6,000 hours per year. That’s nearly two-thirds of the year where the temperature would permit some form of free cooling. Read more...

Energy Efficiency/ Thermal Management Solutions
    
 

Featured Videos
 
 
 

Data Center Advisory Services

Panduit Advisory Services works with you to:

  • Improve performance, availability, scalability, and management of applications
  • Mitigate risks related to convergence, security, safety, and compliance
  • Reduce operating and energy costs
  • Increase ROI relating to physical infrastructure systems
  • Support sustainability efforts

Learn more

Physical Infrastructure Evaluation

Our Physical Infrastructure Evaluation will assess the strength of your physical infrastructure and recommend solutions to ensure that your servers and switches can operate at peak performance.

Learn more

Physical Infrastructure Design Service

Physical Infrastructure Design Service for the data center translates logical network architecture into physical infrastructure design – using a methodology that helps our clients reduce operating costs, speed new hardware implementation, and ensure that future data center growth requirements are considered and properly planned.

Learn more

PIMTM Consulting Services

PIM™ Consulting Services accerates the implementation of the PIM™ Software Platform by leveraging proven and tested deployment best practices and a well-orchestrated methodology to help maximize the value of your investment.

Learn more

On-Site Management Services

Our On-Site Management Services provide the project management that will help you avoid the pitfalls of implementation. To identify and quickly resolve issues as they arise, Panduit’s Solutions Architects take a holistic view of the interplay between the various physical infrastructure systems, the active equipment, and core building facilities. This allows Panduit to identify and assess the adjustments that are needed and to determine the best course of action.

Learn more