Why PAN-STEEL® Stainless Steel Ties are superior in strength!
In the world of cable management, Panduit is a well-known and respected brand. Our products are trusted by professionals across various industries for their quality and durability. One of our most popular products is our Pan-Steel® stainless steel cable ties. These cable ties are highly regarded for their strength, longevity, and are the industry’s standard in harsh environment bundling applications where installation needs to be fast and reliable.
The locking ball mechanism locks the tie in place, once the body is threaded through the head, creating a secure lock. Panduit has tested our metal locking ties to prove our design superiority and performance. Making them an ideal choice for a variety of applications. Watch Here.
What are Pan-Steel® Stainless Steel Cable Ties?
Before we dive into the specifics of Panduit Pan-Steel® stainless steel cable ties, it is important to understand what they are and how they work. Stainless Steel ties are primarily used to bundle and organize cables and wires. Pan-Steel® Stainless steel cable ties are made from high-grade stainless steel, which makes them resistant to corrosion, chemicals, and extreme temperatures. They are designed to securely hold cables and wires in place without slipping or breaking, even under heavy loads.
How Are They Made?
Panduit Pan-Steel® stainless steel cable ties are made from high-quality, DFARS conforming stainless steel. The manufacturing process involves a series of steps to ensure that the cable ties meet Panduit quality standards. First, the raw stainless steel in coils is visually inspected for imperfections and tested for material composition and dimensions to meet our specifications. Next, the heads are stamped on a press and an X-ray vision is incorporated to detect any heads with missing roller balls for quality assurance. The heads are then assembled with a stainless band to produce the finished good which also includes several quality measures and performance tests so that the parts reaching our customers are free of faults. Coated stainless steel ties are either powder coated with polyester or Nylon 11 and a dedicated machine measures uniformity and thickness of the coating. Due to Panduit’s strict quality control, less than one hundred parts per million fails.
What Makes Them Stronger?
There are several factors that contribute to the strength of Panduit Pan-Steel® stainless steel cable ties. The first is the high-quality stainless steel used in their construction. Marine-grade stainless steel is known for its exceptional strength and corrosion resistance, making it an ideal choice for cable ties that will be exposed to harsh environments.
Another factor that contributes to their strength is the design of the cable ties themselves. Panduit Pan-Steel® cable ties are designed with a unique low-profile head (originally patented) that ensures the highest of tensile strengths in the industry and low thread force. The unique locking mechanism ensures a tight grip that will not slip or loosen over time. Additionally, the cable ties are designed with smooth edges that prevent damage to cables and wires. Explore our testing results here.
Why Choose Panduit Pan-Steel® Stainless Steel Cable Ties?
There are many reasons why Panduit Pan-Steel® stainless steel cable ties are the preferred choice of professionals across various industries. Here are just a few:
- Strength: Panduit Pan-Steel® cable ties are known for their exceptional strength and durability. They can withstand heavy loads without breaking or slipping, making them ideal for demanding applications.
- Corrosion Resistance: The high-quality stainless steel used in the construction of these cable ties is resistant to corrosion and chemicals, ensuring that they will last for years even in harsh environments.
- Easy to Install: Panduit Pan-Steel® cable ties are designed for easy installation, making them a popular choice for professionals who need to complete jobs quickly and efficiently.
- Lowest installed cost: Panduit Pan-Steel® cable ties when used with Panduit tools can install three times faster than other solutions in the industry which will result in lower labor and installation cost.
- Global Stocking: Short lead times and strong stock positioning to support time sensitive projects due to Panduit’s vast network of global warehouses.
- Exceptional support: Panduit can provide PPAP, material certs, testing results and other supporting documents at customer’s discretion.
In closing, Panduit Pan-Steel® stainless steel cable ties are an excellent choice for anyone looking for a strong and reliable solution for cable management. With their exceptional strength, corrosion resistance, and easy installation, they are sure to meet the needs and simply installation for professionals across various industries.
For more information on Pan-Steel® Stainless Steel Cable Ties, visit: Stainless Steel Cable Ties & Cable Management - Panduit
- Cable Cleat Selection Made Easy with Panduit Cleat kAlculator
- Why UL Certification Matters for Fault Managed Power Systems
- Field-Ready Playbooks and Building Your Partner Ecosystem
- Why Cable Cleats Outperform Cable Ties for Critical Fault Protection
- NFPA 70e Technical Committee: ONLY Absence of Voltage Testers (AVTs) Meet NFPA 70E 120.6(7)