Panduit Launches SmartZone™ Intelligent UPS Family
SmartZone delivers highly efficient and reliable power protection for IT equipment
Frankfurt am Main, 19.05.2022, Panduit introduces the SmartZone Uninterruptable Power Supply (UPS) family to EMEA region, delivering simple to install and use, highly efficient and reliable power with the capability to integrate into Panduit’s SmartZone DCIM software and provide intelligent systems and environmental alerts, consistent power protection and backup for critical computer ITE. The SmartZone UPS family offers excellent electrical performance, intelligent battery management and long lifespan (with lithium-ion units offering 97 percent efficiency). Compliant with ENERGY STAR® 2.0, EMC, and safety standards, guarantees the SmartZone UPS meets the continually growing power demands of data centre, enterprise, and Edge IT equipment.
The rack-mounted SmartZone UPS family focuses on high reliability, power density, efficiency, and secure manageability. This UPS range offers models with various power ratings, configurations, and battery types to meet application specific needs, and includes 1-3 kVA, 5-10 kVA and 10/15/20 kVA online double conversion units, equipped with powerful and maintenance-free batteries. All SmartZone UPS units offer a 79mm (3.5-inch) touch screen colour display. The screen auto detects the UPS mounting orientation and auto rotates to support horizontal in-rack installation or vertical tower installation.
3-Phase UPS
Developed for critical computer environments, such as data centres and Edge, Panduit’sSmartZone UPS offer an integrated solution with UPS connectivity with multiple externalbattery packs (EBP) and an external Maintenance Bypass Switch (MBS). For larger systemsthe UPS can be configured as 3-Phase In/3-Phase Out high-density UPS, or as 3-PhaseIn/Single-Phase Out high-density UPS. Digital signal processor controlled, the units offersuperior reliability, high power efficiency and constant self-protection and self-diagnostics toprovide maximum system availability. The battery charging current is user selectableallowing the battery charging parameters to be optimise for utilisation and battery life.Furthermore, the system offers innovative three-stage charging to extend service life andguarantee fast charging.
Efficient ECO Mode
The UPS can be manually configured to operate in either normal or ECO mode. Normal mode (on-line double conversion) is the default mode for the UPS unit and operates as a stable pure sine wave AC output and charges the battery. When in normal mode and the load is not critical, the UPS can be set to ECO mode to increase the efficiency of the power supplied.
SmartZone™
As an intelligent UPS solution, the SmartZone UPS can be integrated into common control and monitoring systems, such as the cloud-based DCIM application SmartZone Cloud. This web-based application can manage, monitor and control energy consumption, environmental data, security components, connectivity and IT resources. For secure infrastructure monitoring, the SmartZone Cloud application collects and processes real-time data from the integrated systems and sends timely alerts to prevent potential failures. This allows risks to be efficiently minimised and costly system failures to be prevented.
For more than 60 years, Panduit has been the world's leading provider of innovative solutions in the field of physical and electrical infrastructure for data centers, industrial and building automation and related services. Headquartered in Tinley Park, IL, USA, with offices in 112 locations worldwide, Panduit stands for quality and innovative technologies. The family-owned company with more than 5,000 qualified employees generates sales in the billion Euro range worldwide. Panduit owes its outstanding market position to the constant striving for innovation and the untiring commitment of its employees. The global player invests above average in research and development, in first-class production, in the best possible support of its sales channels and in excellent customer service. This, combined with a strong partner network, is the prerequisite for comprehensive support, sustainability, and solid corporate growth in the networked world of today and tomorrow.