Press Release
Panduit Expands Its Data Center Portfolio with Scalable Direct-to-Chip Cooling Solutions for High-Density AI and HPC Environments
Direct-to-chip liquid cooling addresses the thermal limits of modern AI data centers
Frankfurt am Main, June 2026. The increasing adoption of artificial intelligence (AI), high-performance computing (HPC), and accelerated workloads is driving significantly higher power densities at both rack and chip level in data centers worldwide. Traditional air-based cooling concepts are increasingly reaching their physical and economic limits. With its FlexFusion™ direct-to-chip liquid cooling solutions, Panduit provides an integrated system specifically designed to meet these requirements, enabling efficient, space-saving, and scalable heat removal directly at the source.
Modern AI servers generate high thermal loads directly at the processors. Direct-to-chip (DTC) cooling removes this heat immediately from the chip, reducing reliance on room- or rack-based air cooling. This enables data center operators to realize higher rack densities within existing floor space while maintaining thermal stability.
The Panduit Direct-to-Chip Cooling System consists of FlexFusion DTC cooling racks and rack manifolds made of AISI 304 (V2A stainless steel), developed as coordinated system components. The racks feature adjustable E-rails, double-hinged doors, and electrically bonded steel frames and doors. They utilize previously unused space inside the rack, eliminating the need for additional add-on cabinets or rear expansions. This simplifies planning and reduces potential installation errors when integrating liquid-cooled servers.
The FlexFusion DTC rack manifolds, with a maximum supply pressure of 150 psi (10.34 bar), evenly distribute coolant to the liquid-cooled servers. The heated liquid (recommended: water with 25% propylene glycol) is then reliably returned to the cooling distribution unit (CDU) via 36 distribution couplings. Leak-free quick-connect couplings, automatic air vents, and flexible mounting options support fast, repeatable installation and low-maintenance operation in high-density data center environments.
Panduit’s direct-to-chip solutions are part of a comprehensive cooling portfolio and complement existing concepts such as rear door heat exchangers (RDHx). This enables operators to implement hybrid cooling architectures that accommodate both air- and liquid-cooled systems within a data center and can be adapted incrementally to increasing power requirements.
Panduit’s FlexFusion direct-to-chip cooling solutions are designed for use in AI and HPC clusters, enterprise and colocation data centers, as well as edge and on-premises deployments, helping operators consistently address the thermal, spatial, and infrastructure challenges of modern IT environments.
About Us
Since 1955, Panduit’s culture of curiosity and passion for problem solving have enabled more meaningful connections between companies’ business goals and their marketplace success. Panduit creates leading-edge physical, electrical, network infrastructure and AV solutions for enterprise-wide environments, from the data center to the telecom room, from the desktop to the plant floor. Headquartered in Tinley Park, Ill., USA and operating in 112 global locations, Panduit’s proven reputation for quality and technology leadership, coupled with a robust partner ecosystem, help support, sustain, and empower business growth in a connected world.
Press Contact
Global
Dawn Leach
Manager Global Brand
Tel. 708-532-1800 ext. 81316
Dawn.Leach@panduit.com
EMEA
Patrick-Steeven Skwara
Marketing Manager
Tel. +49 6196 78530-27
Patrick.Skwara@panduit.com
Martin Kandziora
Senior Marketing Manager
Tel. +49 6196 78530-46
Martin.Kandziora@panduit.com