Press Release
Safety Under Full Load: 50 Cable Cleats Put to the Test
Frankfurt am Main, October 2026 — As the electrification of industrial facilities, data centers, utility grids, and buildings continues to grow, so do the demands for the safe routing and securing of power cables. Especially during high short-circuit currents, extreme electromagnetic forces act on cable systems, which, without suitable retention systems, can cause significant damage to equipment and infrastructure. Panduit has now reached an important milestone in the validation of its cable clamp portfolio.
Fifty different cable clamp variants from Panduit have been successfully tested for short-circuit resistance and meet the requirements of the UL-DWMU/7 category currently under development. As a result, a large portion of Panduit’s cable clamp portfolio is already prepared for future market and standards requirements. Additional product variants are currently in the next phase of testing.
Cable Cleats perform a critical safety function in power distribution systems. They secure single- and multi-conductor power cables during both normal operation and in the event of a fault, preventing excessive movement that can result from the magnetic forces generated during short circuits. If cables are not adequately restrained during a fault event, there is a risk of cable movement, damage to cable support systems, consequential damage to electrical components, unplanned system downtime, and, in the worst case, injuries.
The growing importance of high-performance cable restraint systems is closely linked to current developments in energy infrastructure. The expansion of renewable energy, the electrification of industrial processes, charging infrastructure for electric mobility, and the growing number of energy-intensive data centres mean that ever-greater power levels must be transmitted. At the same time, potential short-circuit currents are increasing in many facilities, thereby raising the mechanical stress on cable installations.
For planners, engineers, and plant operators, the proven performance of Cable Cleats is therefore becoming increasingly important. This is because an electrical short circuit leads to a massive increase in current flow through low- and medium-voltage cables in just a few milliseconds. During such events, the current can reach up to 200,000 A. The significant current flow and the resulting increased magnetic field around the cable generate dynamic forces due to the 50 Hz interaction. As a result, the cables begin to vibrate. In the worst-case scenario of a three-phase short circuit, the magnetic-field-induced impact forces between the cables can reach up to 45,000 newtons and develop within 1/100 of a second. Significant damage can occur before the circuit breakers can trip in response to the short circuit. Consequently, cable restraint is crucial for protecting personnel and infrastructure, as well as for minimizing downtime.
Short-circuit tests under realistic conditions demonstrate that a cable clamp system can absorb the forces that occur and maintain the integrity of the installation even in the event of a fault. Such tests provide reliable performance data that supports the sound design and specification of cable management systems.
Regulatory requirements also contribute to this development. National and international standards, as well as electrical engineering regulations, increasingly mandate measures to limit cable movement caused by electromagnetic forces. In many critical applications—such as industrial facilities, power distribution systems, transportation infrastructure, or data centres—validated cable restraint systems are therefore becoming an essential component of modern safety concepts.
For many years, Panduit has been further developing standards and technical specifications for cable management and infrastructure products. In the past, the company’s cable clamp systems have already been tested according to established international standards such as IEC 61914:2021 Ed. 3. For the test environment, Panduit utilized independent, ISO 17025-certified testing, inspection, and certification services (IEEE, IEC, UL, and ANSI) for electrical installations.
The current testing program represents another step toward providing users with reliable evidence for the design of their electrical infrastructure and facilitating compliance with future standards.
To support planning and engineering processes, Panduit also provides digital tools that can be used to determine suitable Cable Cleats and recommended mounting spacings for various applications. This simplifies the design of safe and code-compliant cable retention systems and supports consistent planning from the early stages of a project.
As the expansion of high-performance energy infrastructures continues, the mechanical securing of power cables is becoming an increasingly important component of plant safety. Comprehensive validation programs and standard-compliant testing provide the necessary transparency to reliably select cable management solutions and ensure safe operating conditions over the long term.
About Us
Since 1955, Panduit’s culture of curiosity and passion for problem solving have enabled more meaningful connections between companies’ business goals and their marketplace success. Panduit creates leading-edge physical, electrical, network infrastructure and AV solutions for enterprise-wide environments, from the data center to the telecom room, from the desktop to the plant floor. Headquartered in Tinley Park, Ill., USA and operating in 112 global locations, Panduit’s proven reputation for quality and technology leadership, coupled with a robust partner ecosystem, help support, sustain, and empower business growth in a connected world.
Press Contact
Global
Dawn Leach
Manager Global Brand
Tel. 708-532-1800 ext. 81316
Dawn.Leach@panduit.com
EMEA
Patrick-Steeven Skwara
Marketing Manager
Tel. +49 6196 78530-27
Patrick.Skwara@panduit.com
Martin Kandziora
Senior Marketing Manager
Tel. +49 6196 78530-46
Martin.Kandziora@panduit.com