IntraVUE™ Release Notes
3.2.0 – June 2019
- SNMPv3 support
- Update Server Libraries and embed the JRE
- Install ArpClr Daemon as a service
- Add GUI for updating user credentials
- Mass Move of Devices
- Ability to switch to trial license
- Request and display SNMP sysDesc
- Convert community strings to hive on upgrade to 3.1.3
- Hive v2c entries and legacy community entries shall fallback to v1 if v2c fails
- Show Yellow Connection Lines for Devices with CRC/ifInErrors
- Remove BETA from plant layout
- Warning for wrong top parent
- Improve Security of Login Process
- Remove AutoIP menu items
- Improve change detection
- Update GUI Libraries
- Address Potential Offset Between Event times and Graph times when restoring a database
- Remove FireFox from Installer
- Set file properties of IntraVUE Installer for WindowsSign Installer
3.1.2 – October 2018
- Legend explaining icons and colors added to topology and plant views
- Switch to Switch LLDP rings can be configured for discovery and mapping in addition to Device Level Rings
- CRC data can optionally be collected from devices as well as switches
- Connecting lines turn yellow when there are recent CRC or Input Errors and the lines are highlighted in the Diagnostics View.
- Improved visibility of red and yellow lines when zoomed out
- All main lists now allow list data to be exported
- New filtering capabilities to search and find data in the Events dialog
- Plant view configuration moved to configuration
- Search box gets focus on selection so user does not have to click again
- Improved size of some user interface elements
- Added ability to set the initial zoom level in properties file
- Added ability to change time display between server time and browser local time
- Minor improvements to size of images, user defined text appears when hovering on a device
- Clickable icons show the number of Alarms and Warnings, integrated with search functionality
- Optional software to remove Windows' rebroadcast arp messages included
- Improved error handling during installation and upgrades
- All uses of MAC addresses share a common format
- Added link to online help
- Help dropdown now includes embedded help and online help as well as show/hide Legend
- A new demo database showing the latest IntraVUE features has been added
3.1.1 – June 2018
- New tooltips when hovering over a connection line show port and port descriptions
- Added dialogs to be sure admin is aware of Microsoft Windows ARP bug when scanning local network
- Expanded hover text showing all user defined fields when hovering on a device
- New IntraVUE Export options to simplify usage, Export/Import handles internationalization
- Changes to CRC and InputErrors values are now logged as events and date of last change shown in Diagnostics
- First line of text is selectable, e.g. Device Name instead of IP
- Device List adds all user defined fields, netmask, gateway, mac, vendor, model, and revision data
- Individual device details are provided on a network basis for all KPI data and can be easily edited
- LLDP improvements for special cases
- Email message subject and body are customizable for connection and reconnection
- IP Addresses sorted in order, not alphabetically
- Zoom-to-fit control added as well as other navigation improvements
- Initial plant layout defaults to the same as the topology view
- Minor changes in text font and images at various zoom levels
- Plant view container names are editable
- Additional Interfaces are included in Search and Device List filtering
- Maintaining the screen and topology after logging in
- Prevent move of Unresolved node, moves to Unresolved, and any devices under Unresolved
- Updated code signing certificates
- Added mechanism to disable IP's from using Bridge MIB in advance of discovery
- Fixed bug where only one device's new location was saved when moving descendants in Plant View
- Clarified use message when browser loses connection to IntraVUE server
3.1.0 – February 2018
- Added support for Active Directory (AD)
- Support for HTTPS has been added
- Initial support for Profinet-based device level bus and ring topologies using LLDP communications
- The Q-Mib is now supported for getting topology data from switches when the Bridge Mib is not supported by those switches
- In addition to normal daily backups, backups are made at 12am, 6am, 12pm and 6pm so one minute resolution data is available for analysis beyond the current database
- Port Descriptions (FastEthernet0/2) are displayed for connecting lines in addition to the internal port numbers previously displayed
- German, Chinese, Japanese, Russian, and French languages have been added in addition to Spanish and English
- Vendor names are shown for all devices, not just Ethernet/IP devices
- Global event log and Device sidebar event log searches now fetch data from server instead of within the original results making analysis easier
- "KPI" is now integrated into the main User Interface
- The KPI user interface now shows statistics by network and devices within a network
- A new List View is added which provides a list of all devices (filterable) and provides ability to edit the device name, critical device state, and admin verified state within the list
- A dropdown list of local interface IP addresses is shown in the scanner configuration tab when using the local computer as the top parent (similar to IV2)
- CRC and/or Input Errors as well as port and port descriptions are shown for devices supporting the standard MIBs in new diagnostics sections - in the sidebar for a single device and under view for all devices
- IP Address has been added to the sidebar header text, under device name so it is always visible when scrolling the sidebar
- Multiple devices can be deleted in one operation
- Device names have been added next to their IP Addresses under sidebar graphs when in Aggregate mode
- Improved handling of Internet Explorer's compatibility mode settings
- When the Ultra or Fast speed is selected in the scanner tab a warning message warns users about the risk to very old PLCs having small memory and slow processors
- The Archive function has been moved from Advanced to Database, next to Export/Import
- The Help files are now part of the distribution and available in isolated systems
- Updated to latest versions of underlying tools and IntraVUE now complies with several Windows, Linux, and Apache security hardening specifications
- Fixed minor bug which removed registration text on loss of communication
- Hyperlinks to navigate to a device added to Diagnostic, Event Log, Device List View, and KPI details
- Initial discovery of devices has been slowed until it has been verified that the host IP is not the top parent of any network containing legacy equipment susceptible to frequent ARPs
- When configuring images for a device, you can enter or paste text to more easily navigate through the image list
- Minor bug fixes
3.0.2 – August 14, 2017
- Send an email when a device reconnects if an email was sent saying it disconnected
- Zoom level increased so IP address is distinguishable when many devices are on the same switch. At intermediate zoom levels, the wireless device dashed lines are now more visible.
- Caching of KPI data fixed so latest statistics always display
- In KPI Supervisor, email is now an optional field
- In KPI Supervisor, caching of data fixed so latest statistics always display
- Internet Explorer compatibility mode automatically set appropriately for both IntraVUE v2 and IntraVUE v3
- On an upgrade, Installer now makes a backup and restores the backup to maintain the previous online/offline status
- Automatically check for database corruption and if corrupt, notifies the user and provides an option to attempt backup the database
- Insert an event log entry when a database is restored
- Internationalized date format for English option
3.0.1 – July 24, 2017
Major Updates
- Spanish language has been added to the user interface
- Demo database and supporting files have been added
- Added new Quick Filters such as only highlighting critical devices, just switches, only disconnected, etc.
- When using filters, search only finds devices matching the filter(s)
- Added IP of top parent to Network Name in Filter Dialog
- Ghost node line colors changed from red to black
- Image used for switches made dark for better contrast
- Styling of 'enabled' buttons improved
- Added international paper sizes for Plant Layout
- Aggregate data is now available for any device with children
- Entering '*' in search box returns all devices
Minor improvements and bug fixes
- The zoom level at which images appear changed is one step further zoomed in
- Ping failure graph changed to always reflect 100%
- Ping and Bandwidth graphs now have same width and vertically align
- SNMP community removed from visibility when not logged in as admin
- Fixed issue between mouse pointer and mouse rollover
- In Plant Layout connections that are within a container are now selectable
- Fixed email notifications to refer to IV3 not IV2
- Fixed bug where a deleted device's previous events were visible if rediscovered
- Added more information if an obsoleted product key is used in registration
- External links open in a new tab
3.0 – June 12, 2017
- New User Interface based on HTML5 (no need for Java support in the Web browser)
- New Plant Layout View allowing physical placement of devices at their locations in a drawing of the plant
- Ability to easily show only selected networks
- Topology drill down with bread crumbs
2.4.1 - August 18, 2016
- Improved handling of Network Address Translators
- Introduction of KPI Supervisor which collects data from multiple remote IntraVUEs and consolidates KPI data
2.4.0 - December 28, 2015
- Added Critical Performance Indicator (KPI) reports which will track and graph 3 parameters associated with critical devices:
- Average uptime in 24 hour increments (for always-on devices)
- Number of events associated with edge devices in 24 hour increments
- Number of events associated with switches in 24 hour increments. This feature is the first to use HTML5 and requires modern browsers. It is the start of removing use of Java in the IntraVUE user interface.
- Service Contract Validation code mechanism introduced as part of the registration dialog. The KPI feature only runs on systems under current support contracts.
- Appliance software update process improved.
- Firefox installer now bundled as a convenience.
- Added property to ivserver.properties file, trapmailer.service, to allow suppression of trapmailer.
- Added user feedback if product key is detected as being obsolete during registration.
- Fixed faults resulting from SNMP device changing interfaces and prevent children of lost interfaces from becoming detached.
- Improved auto IP handling of its restarts.
- Updated IntraVUE logo.
2.3.0a16 - February 24, 2015
- Changed scanner's messaging algorithms to be more efficient for very large networks.
- Increased memory available to the scanner in very large network scanning situations.
2.3.0a14 - February 9, 2015
- Java certificates renewed for new 5-year period, certificate in previous versions expired in February. Most IE 11's and Java 8 will not work with previous versions.
- Fixed 10 GBit switch ports causing repeated events of port speed changes.
- Fixed security issue in some JSP pages. (NCCIC/ICS-CERT advisory ICSA-15-057-01)
2.3.0a11 - September 22, 2014
- Signed some additional applets. Set applet to 'all-permission' to allow copy/paste.
- Obsolete throttle.jsp
- Allow the agent to collect cipscan data.
- Fixed 'all red lines' issue caused by ICMP TTL responses.
- Minor changes/tweaks to discovery tool of the agent/plug/appliance.
2.3.0a2 - June 30, 2014
- Created process to upgrade plug and appliance software remotely.
- Made changes so that IntraVUE works with Java 7 better on both the host and client browsers.
- Most applets are now signed.
2.3.0 - June 5, 2014
- Improved feedback from submit operation of registration dialog.
- Created new checkbox 'restore offline' to make it easier to restore online and avoid problems using the former extra dialog asking 'do you want to be in offline mode'.
- Added advance options to System Menu.
- Added ability to auto-adjust ping thresholds for devices over the threshold.
- Added ability to delete all Red Filled boxes designating admin verified devices which have moved.
- Allow user to select which views to appear in the hover text using the existing General Tab of System Configuration.
- Fixed bug handling thresholds for devices that existed in multiple networks.
- Suppress erroneous readings of Threshold greater than 100% based on reporting problems with some devices.
- Show a red line to switches which are not responding to pings. Previously if any device below a switch responded, then all the lines 'above' it would be green.
- Ensure plug and appliance retain time and timezone settings after an upgrade.
2.2.0b5 - 2.2.0b22 January through June 2014
- Fixed bug which prevented deleting devices which were in multiple networks (e.g. VLAN switches).
- Implemented encrypted admin passwords for the web server (Tomcat) with a web page to help to encode.
- Created 3 more user defined a set of properties. The Ethernet/IP data previously using UD1,2,3 will be moved to UD4,5,6. UD4,5,6 named Version, Vendor, Model.
- Reduced disk wear on plugs and appliances with software and memory changes.
- Modified trunkingdefs.txt file so VLANs can be restricted on a per switch basis, rather than globally.
- Refine handling of MAC changes to better support DHCP systems. Events recorded before change of IP are now associated with the new IP
- The help page for dongle based product key upgrades put back in.
- Added a new Critical classification for devices so they can be assigned to an unknown, ignored, critical always on, and critical intermittent states. These states are used to produce Key Performance Indicator reports in optional software.
2.2.0b4 - October 24, 2013
- Fixed initial state after upgrade so scanner is online.
- Added configuration utilities for IntraVUE Plugs to edit files and put putty and winscp in plug's tools folder
2.2.0b - October 7, 2013
- Generate a better choice of IP address to use for the link back to IntraVUE in email notifications (not 127.0.0.1).
- Fixed bug caused by rapidly deleting many nodes in the browser.
2.2.0 - September 15, 2013
- Link Speed - show the current link speed in the Threshold Line dialog. Create events any time a device changes link speed. This helps identify devices that may need to be fixed speed due to dropouts when auto-negotiating.
- Fix - ensure a device which loses SNMP and has a red outline, gets a green outline when SNMP returns (previously required an apply operation).
- Add a description (IP address) of deleted red box node in the event log.
- Ensure all nodes for a given IP are updated for attribute changes when any one changes, for instance, a switch in multiple VLANs.
- Dynamically update Ethernet/IP data instead of only upon discovery. Unverify admin verified devices if there is a change in its Ethernet/IP data for vendor, model, or software version to make the change easily noticed by a user. Record event in event log.
- Reduce mac address changed events when routers utilize redundant protocols such as HSRP and VRRP.
- Added ability to easily set/change time and time zone for the plugs in the plug discovery tool.
- Improved user feedback when using the Generate Support Archive dialog and the Registration dialog.
- Fixed problem where transmit and receive bandwidth values were sometimes reversed compared to their respective graphs in the Threshold Line Dialog.
- Removed automatic WAP detection which sometimes set layer 3 switches as WAPs.
- Fixed problem that caused the new location of an admin verified device to remain a blue filled box, it is now a tan filled box as intended, making it easy to see in the user interface.
2.1.0e10 and e13- April 25, 2013
- An additional method of registration / licensing that does not require the use of a dongle has been added for use in Virtual Machines or in cases where a dongle driver causes issues.
2.1.0e8 - October 3, 2012
- Devices are queried to see if they support the CIP protocol of Ethernet/IP and if they do, put the vendor name in user defined 2 and the model number in user defined 3, when these do not already contain a name.
- Fixed bug where comma separated email names caused an exception when sending the test email.
2.1.0e6 - July 12, 2012
- Made changes so JRE 1.6 is installed even when JRE 1.7 already exists to avoid incompatibilities between JRE versions.
2.1.0e4 - May 30, 2012
- The n/a and N/A nodes now have unique numbers appended to make it easier to search and correlate threshold data.
- The dongle is checked for continually, so it is no longer necessary to do Apply/Close for the scanner to notice.
- The bug where the viewname was showing as 'User Defined 1' etc. even when overridden (when using a URL like '?v=3') is corrected.
2.1.0e2 - March 8, 2012
- The supervisor has a 'broken' icon if the remote MySQL is stopped.
- Webserver suppresses search for web links of devices with manually set web links.
- Registration authentication code changed.
- Increased width of the IP field in the search dialog.
2.1.0d - November 17, 2011
- Peak Values are now the initial, default values for the line and multiple thresholds dialogs.
- Default scan range now goes from 1 to 254 instead of 0 to 255 in the scanner tab's network setup dialog. This is because we are finding more devices that actually and mistakenly respond to the broadcast address.
- Added a 'depth=N' parameter to the IntraVUE URL to cause all nodes beyond that depth to be initially displayed collapsed.
- Fixed bug where ARP data from virtual router was ignored because the upstream MAC was not recognized.
- Changes to MySQL settings to increase memory. Note: when upgrading we suggest always reinstalling MySQL.
- Changes in IntraVUE Plug software to improve memory usage and minimize disk writes.
- Changed IntraVUE Supervisor to show the current state of Admin Verified devices only. Previously any device could affect the state and the state only changed after acknowledgment.
- Change device names to favor Netbios names over SNMP names to avoid repeated 'name changed' events.
- Change bandwidth data to favor a managed switch as the source of the device, for more reliable data.
- Made improvements to decrease the time it takes to get SNMP data from a managed switch by more than an order of magnitude.
- The IntraVUE installer no longer requires the dongle during installation.
- Minor fixes to dongle discovery mechanism.
- Minor changes to Supervisor event collecting.
- Minor improvements in the scanner.
2.1.0c - April 13, 2011
- IntraVUE Plug - most changes in the c release relate to the introduction of this new Linux based product.
- Supervisor module - Fixed memory leak and event handling when a satellite IntraVUE's database is restored.
- Added logic to purge even some non-repetitive events from the event log.
- The installer uses admin mode in all cases.
- Fixed bug (starting at 2.1.0b) where a pingable IP is not discovered when the scanner could not find a mac, e.g. remote devices without a router's SNMP.
- Added tools/util.jsp to allow remote switch probe, ping, and tracert from IntraVUE host via a web page.
- All devices in an IntraVUE network are deleted with the network is deleted in the System Config dialog's Scanner tab. (The events remain)
- Auto IP ignores IntraVUE settings for auto IP in offline databases.
- Made sorting of the icons and thumbnail image names case insensitive when browsing for images.
- Added change of name to the event log, and also to event purging list.
- Refined and improved handling of 'generate support archive' to avoid security issues in the browser.
- Fixed bug which could cause continuous automatic backups for monthly backups.
- Improved merging of top parent's auxiliary IP addresses.
2.1.0b - October 18, 2010
- Support added for the newly released "IntraVUE Plug - Network Scanner/Recorder".
- Added more logic to handle extremely unusual RSTP ring reversal use cases.
- Fixed bug which occurred when a device was in more than one IntraVUE network and it was deleted in one, it would reincarnate itself even if it was no longer in that network's scan range.
- Ensure the scanner clears its memory of the bridge mib for a disconnected switch.
- Fixed SQL exception on optimized threshold logic.
- Fixed use of forward slash and backslash characters in support property files.
- Implemented a new feature for netbooks and technician laptops that automatically configures a new top parent and starts scanning a new network every time the host computer gets a new IP address. Any previous, meaningful data is automatically saved using logical file names before the new scan starts.
- Adjust scheduling of statistics to minimize MySQL InnoDB writes and wear on flash memory.
- Fix problem where an internal Interface could have a mac address but no ip address.
- Fixed bug where email authentication was being lost because a wrong index had been used in the database.
- Fixed bug causing erroneous IP address changes when the MAC address was not known.
- Adjusted size of dialogs for netbook screens.
- Removed momentary 'license exceeded' message when restoring a database.
- Fixed checking for Admin privileges on Windows 7 type machines.
2.1.0a - June 23, 2010
- Added new USB dongle drivers to handle Windows 7.
- Avoid problems when there are multiple versions of the Java Runtime Environment
- Fixed bug where peak values were not correctly calculated for the 15 to 30-hour data.
2.1.0 - June 8, 2010
New features
- Support 'intravue agent' which allows remote scanning of networks.
- Introduce 'network group' concept to handle the case where multiple private networks have the same IP ranges.
- Record both peak and average values of ping and bandwidth to make it more convenient to troubleshoot issues older than 6 hours.
- Network selection URL now explicitly 'shows' networks as well as 'hiding' them.
- Add 'link comment' facility which allows users to document wiring, unusual port numbering, ports of unmanaged switches, or any other text to appear as part of a connecting line's hover text.
- Arrange that the event log is systematically 'trimmed' to remove repetitive messages for a single device, resulting in much smaller database files.
- Trapmailer and ivserver are now combined so that traps can be configured to update Modbus/TCP registers.
- Add 'user archive' facility, where an enhanced system snapshot is taken and may be automatically transferred to an FTP server or user's browser.
- Add French language help.
- Implement facility to allow agents on a network to be discovered regardless of IP address and have IP settings reconfigured.
Minor Improvements and Bug Fixes
- Allow ghost node (red boxes) to be found in 'search by IP'.
- Installation defaults to c:\intravue, not c:\program files\intravue but will re-use existing installation directory if found.
- Corrected bug which caused incorrect behavior when adding more than one network at once.
- Arrange that the list of networks and scan ranges entered is kept in order of insertion.
- Save all important user files and restore as part of an upgrade. Uses series of backup folders, 'prev0000' etc.
- Allow merging of user-entered changes to a new ivserver.properties when upgrading version. Also, retains site license header.
- Warn user to make a backup before performing an upgrade.
- Correct focus issues on entering a password (cursor already in the correct field).
- Improve default settings for trapmailer.xml so they are benign.
- Avoid SQL exceptions when recording thresholds after a host computer system time change.
- Tune innodb parameters to avoid performance problems with larger databases and limited memory.
- Avoid change of MAC messages when using a virtual router.
- Correct bug which occasionally failed to detect missing devices.
- Fix Pelco DVR bug which was adding IP cameras to the wrong network.
- Arrange for Pelco and Supervisor software to be delivered on standard CD.
- Improve export/import to break out columns, suppress update if column empty.
- Arrange that MySQL, ivserver, tomcat services auto-restart after any failure.
- Block attempts to perform the manual move from one IntraVUE network to another.
- Remove arbitrary 100% limit on bandwidth thresholds.
- Support user-modifiable system default settings for threshold values.
- Avoid spikes in multiple threshold graphs after 'apply/close' by using interpolation.
- Handle situation better where a link on display has threshold data from both parent and child. Adjust both, suppress one.
- Support multiple email addresses on device disconnect.
- Arrange that 'backup' can be done without requiring admin privilege.
- Avoid permanent ghost nodes on ring reversal by clearing 'admin verified' marker if a device is detached to avoid circular structure.
- Ensure large trap messages are truncated appropriately to store in the event log.
- Ensure displayed thresholds have consistent time ranges.
- Allow direct upgrade of systems from previous full release only (2.0.5). Otherwise prompt for explicit uninstall first.
- Enhance 'data not current' warning on graphic display to indicate the probable reason, specifically loss of dongle.
- Improve license count detection and display.
- Arrange to pre-purge very large databases at the time of restore to avoid excessive memory use at startup.
- Change applet jar file names on each release to avoid Java cache issues on client browsers.
- Improve timeout mechanism for JAVA detection to allow for slow startups.
- Make oidval table purge timing adjustable, not fixed 60 secs.
- Upgrade dongle driver to work with Windows 7.
- Switchprobe.jar given a main-class attribute to allow double-clicking.
- Change the name of UD3 from 'Diagnostics'.
- Only use 'wasPinged' interface when sending SNMP requests.
- Install should block if the old version of MySQL is present and require a manual removal.
- Microsoft deliverable file msvcr71.dll is placed in the launch directories auto IP and auto IP/tomcat6/bin to withstand frequent JRE updates.
2.0.5c - May 7, 2009
- The Top Parent IP address is automatically added to the scan range of a network if not already added.
- Fixed 'Enable AutoIP' checkbox on the Device Configuration dialog so the device gets correctly added to Auto-IP.
- Fixed problem where 'public' was configured as the SNMP community for all devices without a community when Apply and CLose is executed.
- Added ghost nodes (Red boxes with dashes in the IP) to the Search results so you can easily find the current and previous location of a device.
- Minor bug fixes.
2.0.5 - February 17, 2009
- Handle Cisco Virtual routers having MAC addresses which are not in the router's list of interfaces.
- Allow installation by Domain administrators.
- Avoid exception of a device and its parent is manually deleted within the same scan cycle.
- Prevent screen update before a restored database is fully restored.
- Removed some MySQL operations which caused some dialogs to take a very long time to display.
- Ensure consistent SNMP, bandwidth, and ping data for devices, such a switches, that appear in more than one IntraVUE network.
- Avoid a problem which could cause the threshold data to grow without being averaged, resulting in huge database files.
- Revised import/export function to include all the checkboxes on the Device Configure dialog.
- Implemented feature to disable SNMP data for name and location of a device. Added ignoring the bridge mib and all SNMP.
- Provide the ability to learn MACs from switches, avoiding the need to access a router if only switch macs are needed.
- Avoid spurious event log entries if a device is disconnected and then the database is restored and the device is still disconnected.
- Ensure consistent reported of interfaces for routers that appear in more than one IntraVUE network.
- Allow a device to be designated a 'managed hub' in which case all its peers will become children. Intended primarily for Wireless Access Points, but also useful for web-managed switches, Virtual Machines, and other situations.
- Handle the case where a Layer 3 switch is a top parent and it is also switching.
- Allow suppression of SNMP name and location data.
- Do not record SNMP community for a device until a successful snmp operation.
- All devices under a Wireless Access Point will have dashed lines.
- Allow for more control of email alarm messages in the subject line and the body.
- Automatic detection of Wireless Access Points (WAP) that support the 'wireless mib'.
- Automatically check a device under a WAP as having 'auto connect' properties.
- Import function updates all instances of an IP address instead of just the first.
- Added new event log entries for trunkingdefs.txt file and scanner version.
- Fixed a problem where an import or an apply operation close to a one-minute boundary caused all the threshold data to have a 'dip to zero'.
- Provide a scanner speed control in the System Configuration's Scanner tab.
- Prevent ghost nudes (red boxes) from being improperly promoted up the topology.
2.0.4 - Sept 23, 2008
- Device no longer remains in unresolved if its mac was provided by an external network before its real subnet parent.
- Handle devices with multiple IP addresses using any of them, remembering the canonical one as the one in the scan range, but allowing placement if any interface is known by subnet parent.
- Ignore phantom 0.0.0.0 IP addresses.
- Avoid multiple SNMP scans using different IPs of the same device, ensure mib consistent.
- Allow scanner arp data to be unconditionally used even if the scanner is not the top parent.
- Improve handling of V2 TOOBIG response, retrying at V2 with reduced OID count, not allowing drop to V1 (HP switches)
- Speed up database restore using alter-db-fast.sql.
- New, HTML based help system
- Fixed too many devices being displayed in Multiple Thresholds dialog.
- Allow top parent to be deleted.
- Clean up delete node events.
- Log changes of uplink port.
- Report port changes for top parent mac in the event log.
- Correct network status mechanism in ivserver.xml for changed case of network join message.
- Ensure ping threshold events are reported correctly.
- Suppress ping fail % events.
- Arrange to log threshold events.
- Fix bad jre message if install dir not writable.
- Add event log msgs for manual add/remove.
- Allow both :i and :w in ivserver.xml.
- Avoid noroutetohost if no default gateway.
- Merge device and transfer properties and names if IP change detected.
- Avoid duplicating adjustAutoInsertedNodes when multiple networks.
- Avoid change of SNMP state while device disconnected.
- Suppress threshold reports where the device is disconnected.
- Ensure import changes to device name and location are not overridden by the scanner.
- Changed database MySql structure from isam to InnoDB and implemented protection for the MySQL tables from sudden power loss.
- Added trunkingdefs.txt to handle trunked switches and relabeling of switch ports if needed.
- Provide the ability to hide selected IntraVUE networks in the browser display.
2.0.3 - May 10, 2008
- Support for Java 1.6
- USB Dongle support for 64-bit Windows
- Red SNMP lost outlines are not created due to incorrect responses, only no response
- Suppress moves on false reports (when detected) from some switches
- Prevent promotion of disconnected devices is rare cases
- Node selected color changed from Red to Blue to avoid confusion with red SNMP lost outline
- Fixed linkage between IntraVUE and AutoIP regarding the Auto-IP check box in Device Configuration
- Default view to display, icon state, and thumbnail state can be set in ivserver.properties file
- URL query string can center a device, email alarm centers the device in the alarm state
- Email alarm data now includes device name and alarm cause
- Fixed minor installation bugs
- URL added to allow reading of detailed log file from remote PC
- Fixed problem where some applet windows 'hung' and the user only saw a white filled dialog
- Resizing of child windows improved
- Added site license support
- Added new icon images
- Don't report switch from SNMP V2 to V1 as a loss of SNMP
- ivserver.properties file added scanner.switch.move.deferral.count to overcome bad switch issues
- Event Log - disable options that have not been implemented
- Device Configure Image Tab's browse button will find image files regardless of case
- Multiple Threshold Graph improved to display many devices at 100% ping failure
- Multiple Threshold Graph time scale display made the same as the Connecting Line Threshold Graphs
- Multiple Threshold Graph added '0' data points for missing times
- Check for disk drive based key codes removed from installer
- Search now supports the * and ? wild cards
2.0.2 - November 30, 2007
- Improved methods of getting SNMP data from switches and routers to reduce traffic and improve scan times
- A warning message displays on the browser if the threshold data is older than 3 minutes
- New Search dialog searches all view names and MAC addresses
- Improved display of devices under auto-inserted nodes
- User information and number of discovered devices display in the General Tab of System Configuration
- Device names are displayed in addition to IP address in the Event Log and the Multiple Devices Thresholds
- Multiple Threshold Line Dialog can be configured for the number of devices to display
- Multiple Threshold Line Dialog additionally converts bandwidth data into transmitted and received bytes
- Backup location cannot be changed.
- Site licensing implemented which does not require use of a USB dongle
- Cisco VLANs can optionally be constrained to a list of VLAN numbers
- Installer improvements
2.0.1 - September 4, 2007
- NetBIOS names discovered.
- Improved handling of Wireless Access Points
- Scanner log files made configurable for location and size.
- Test Email button added.
- Settings in ivserver.properties file allows configuration of scanner ping and snmp queries
2.0 - May 11, 2007
- Major decrease in use of host computer resources.
- Major decrease in SNMP queries to devices.
- Automatic handling of Cisco VLANs.
- Integrated into Apache Tomcat eTomcat web server
- All admin functions can be performed remotely including restore and network configuration
- Threshold graphing for multiple devices at the same time
- Vastly improved Event log functionality
- The old 'Show Status' as a web link in User Defined 3 mode is now a regular menu item in all views called 'SNMP Data...'
- System Configuration
- Better top parent selection
- Easy display of registration and registration information
- Documentation implemented using WIKI technology so users can edit and add information
- New method of selecting devices
- System Configuration
- Automatic backups
- Email - send test email button
- Device Configuration
- Single Tab to edit all thumbnail and icons
- Single Tab to edit all web links
- Single Tab to edit all view names
- Device Properties will have all the web links for all views
- License node count will be based on discovered nodes with IP addresses, not all nodes
To access help files, visit panduit.com/intravuehelp.
To contact Technical Support, email techsupport@panduit.com or calling 866-405-6654.