Sustainability Considerations with Multimode Fiber
With sustainability and environmental issues top of mind, individuals and businesses are doing what they can to limit their environmental impact and reduce their carbon footprint. Although many people are more conscious about how their actions impact the environment, there are things that we still take for granted or do not think about.
One of those areas is cabling infrastructure.
Are you considering ripping out your old multimode fiber backbone and replacing it with singlemode fiber?
Think again. What are you going to do with the multimode fiber cabling that you remove from your building? After pulling out the old multimode fiber, you could throw it away, along with the other waste and leftover materials created from the rip-and-replace project. All that multimode fiber will then wind up in a landfill, and here’s the problem: no one knows how long it will take for multimode fiber to decompose. Some feel it could be hundreds of years.
Recycling as an Option
Can multimode optical fiber be recycled?
It depends on where the project is geographically located as it requires a specialized recycler. It’s not as simple as throwing multimode fiber into the blue recycle bin and expecting it to be recycled. Exactly how much of the cable is recyclable depends on the makeup of the cable. The cable’s jacket and armor can be ground up and recycled, but what about the reinforcing strands of Kevlar®? Even if some of the multimode cable’s components can be recycled, not all of them can be.
When it comes to sustainability, ripping out the old multimode fiber and replacing it with singlemode fiber is not very sustainable.
The More Sustainable Approach
There is a sustainable alternative to ripping and replacing existing multimode fiber: OneMode™.
Panduit’s OneMode offering is a device that allows singlemode optical modules to be used with an existing multimode fiber backbone. OneMode works by shaping the singlemode laser light so that when it launches into the multimode fiber backbone, it uses only the fiber’s fundamental mode. This means that the multimode fiber is behaving as if it were singlemode fiber. All the modal and chromatic dispersion limitations that exist with multimode fiber disappear.
Installation is quick and straightforward. Deploying OneMode only requires access to the ends of the legacy multimode fiber. The fibers can be upgraded within hours with minimal disruption to operations. Given that OneMode takes much less time than a rip-and-replace project, it is less expensive to deploy.
OneMode is the sustainable, environmentally friendly, and economical way to upgrade your existing multimode fiber backbone.
- Cable Cleat Selection Made Easy with Panduit Cleat kAlculator
- Why UL Certification Matters for Fault Managed Power Systems
- Field-Ready Playbooks and Building Your Partner Ecosystem
- Why Cable Cleats Outperform Cable Ties for Critical Fault Protection
- NFPA 70e Technical Committee: ONLY Absence of Voltage Testers (AVTs) Meet NFPA 70E 120.6(7)