プレスリリース
Single Pair Ethernet connector standard published by IEC
TINLEY PARK, Ill. — (June 3, 2020) — Panduit, a global leader in innovative electrical and network infrastructure solutions, is pleased to announce the approval of the IEC 63171-1 (Variant 1) Single Pair Ethernet connector style by ISO IEC SC48B, the standards body that helps with international standardization of low voltage connectors.
This newly standardized Single Pair Ethernet connector design will be key to supporting the explosion of Ethernet connectivity into edge devices within a broad range of applications including industrial controls, building automation systems and related sub-systems that can take advantage of structured cabling. The connector supports shielded and unshielded variants and has been proven to show high resistance to electromagnetic interference. Those unfamiliar with low voltage electronics will find the connector design easy to install, enabling a sensible migration path towards Ethernet for IoT and Industry 4.0.
For more information about Single Pair Ethernet expands automation system possibility, read the “Reducing the barriers to Anything is Possible” blog post on the Ethernet Alliance website.
パンドウイットについて
1955年以来、パンデュイットの探求心と問題解決への情熱は、企業のビジネス目標と市場での成功との間でより意味のあるつながりを築いてきました。Panduitは、データセンターからテレコムルーム、デスクトップから工場フロアまで、企業全体にわたる環境向けに、最先端の物理的、電気的、ネットワークインフラストラクチャおよびAVソリューションを提供しています。米国イリノイ州ティンリーパークに本社を置き、世界112カ所で事業を展開するPanduitは、品質と技術リーダーシップにおける確固たる評価と、強力なパートナーエコシステムを組み合わせることで、つながった世界におけるビジネス成長の支援、維持、促進に貢献しています。