Panduit Honored in 2021 Cabling Installation & Maintenance Innovators Award
Panduit, a global leader in innovative electrical and network infrastructure solutions, was recognized today with five Cabling Innovators Awards in the 2021 competition. Cabling Installation & Maintenance bestows the Innovators Awards annually to the best products and projects in the industry.
Panduit received five awards in total, including a Platinum honor for Single Pair Ethernet (SPE) solution, a seamless single protocol network from application edge to the cloud. SPE simplifies network design and operation, eliminating the support and translation of legacy network protocols used in OT networks.
“With the emergence of Single Pair Ethernet technology built for OT applications, we expect to see accelerating growth in wired Ethernet in place of fieldbus and analog communications,” states Mike Vermeer, Engineering Development Strategy Manager. “Panduit is grateful to be recognized for our efforts to bring this technology to market, and we are excited for the possibilities this brings to intelligent buildings, smart factories and Industry 4.0.”
Panduit also received two Gold awards and two Silver awards:
• FlexFusion™ Cabinet (Gold Honoree) - Offers a unique universal platform for all types of data centers and servicing needs including Hyperscale, Edge and Colocation. The cabinet is built with best-in-class weight load of 3,500 lbs., doors with maximum air flow of 80%, and custom configurations to meet network needs.
• PanZone® TrueEdge™ Wall Mount Enclosure (Gold Honoree) - With 0 RU vertical patching, the enclosure’s mounting method minimizes network infrastructure investment by providing a solution to eliminate a rack or cabinet.
• TX6A™ FieldCord™ Connectors (Silver Honoree) - Enable connection to devices in the most confined cable routing paths and has the capability to be re-terminated up to 20 times with no additional parts.
• Adjustable Depth 4-Post Racks (Silver Honoree) - Combines the stability of a cabinet with the accessibility of an open rack to provide users with maximum flexibility when designing the network layout.
“Helping customers gain competitive advantage and ensuring their utmost satisfaction is a core focus for Panduit. Taking the time to understand each customer’s unique infrastructure needs has helped us to innovate new products that will allow them to grow in this ever-evolving, modernized world,” states Marc Naese, Senior Vice President of Network Infrastructure. “Receiving five CI&M Innovators Awards is an honor and we are incredibly thankful for the recognition.”
For more information, click here to visit Cabling Installation & Maintenance’s website.
About Panduit
Since 1955, Panduit’s culture of curiosity and passion for problem solving have enabled more meaningful connections between companies’ business goals and their marketplace success. Panduit creates innovative electrical and network infrastructure solutions for enterprise-wide environments, from the data center to the telecom room, from the desktop to the plant floor. Headquartered in Tinley Park, IL, USA and operating in 112 global locations, Panduit’s proven reputation for quality and technology leadership, coupled with a robust partner ecosystem, helps support, sustain, and empower business growth in a connected world. For more information, visit www.panduit.com.
- AI-Powered Data Centers: Balancing High Performance with Sustainability
- Broadband 2026 Panduit Experts Predict What’s Next
- Real World Benefits of Deploying VSFF Solutions with Gen7 SAN Directors
- TX6TM-ER Cable Surpasses 100-Meter Limit for Reliable Network Performance
- What’s Your Logistics Playbook for the Broadband Fiber Boom