Skip to main content
globe
地区和语言 {{(header.eyebrow.langSelector.label != '') ? header.eyebrow.langSelector.label : getTranslation('panduit.localeselect.chooselanguage')}}
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
Panduit Honored in 2021 Cabling Installation  & Maintenance Innovators Award

 

TINLEY PARK, Ill. — (August 31, 2021) — Panduit, a global leader in innovative electrical and network infrastructure solutions, was recognized today with five Cabling Innovators Awards in the 2021 competition. Cabling Installation & Maintenance bestows the Innovators Awards annually to the best products and projects in the industry.

Panduit received five awards in total, including a Platinum honor for Single Pair Ethernet (SPE) solution, a seamless single protocol network from application edge to the cloud. SPE simplifies network design and operation, eliminating the support and translation of legacy network protocols used in OT networks.

“With the emergence of Single Pair Ethernet technology built for OT applications, we expect to see accelerating growth in wired Ethernet in place of fieldbus and analog communications,” states Mike Vermeer, Engineering Development Strategy Manager. “Panduit is grateful to be recognized for our efforts to bring this technology to market, and we are excited for the possibilities this brings to intelligent buildings, smart factories and Industry 4.0.”

Panduit also received two Gold awards and two Silver awards:

  • FlexFusion™ Cabinet (Gold Honoree) - Offers a unique universal platform for all types of data centers and servicing needs including Hyperscale, Edge and Colocation. The cabinet is built with best-in-class weight load of 3,500 lbs., doors with maximum air flow of 80%, and custom configurations to meet network needs.
  • PanZone® TrueEdge™ Wall Mount Enclosure (Gold Honoree) - With 0 RU vertical patching, the enclosure’s mounting method minimizes network infrastructure investment by providing a solution to eliminate a rack or cabinet.
  • TX6A™ FieldCord™ Connectors (Silver Honoree) - Enable connection to devices in the most confined cable routing paths and has the capability to be re-terminated up to 20 times with no additional parts.
  • Adjustable Depth 4-Post Racks (Silver Honoree) - Combines the stability of a cabinet with the accessibility of an open rack to provide users with maximum flexibility when designing the network layout.

“Helping customers gain competitive advantage and ensuring their utmost satisfaction is a core focus for Panduit. Taking the time to understand each customer’s unique infrastructure needs has helped us to innovate new products that will allow them to grow in this ever-evolving, modernized world,” states Marc Naese, Senior Vice President of Network Infrastructure. “Receiving five CI&M Innovators Awards is an honor and we are incredibly thankful for the recognition.”

 

For more information, click here to visit Cabling Installation & Maintenance’s website.

关于 Panduit

自 1955 年以来,Panduit 的进取精神和解决问题的探索热情帮助许多公司在业务目标与市场成功之间搭建起了桥梁。Panduit 为从数据中心到电信机房、从台式机到工厂的各种企业级环境创建领先的物理、电气、网络基础设施和音视频解决方案。Panduit 总部位于美国伊利诺伊州廷利公园,在全球 112 个地区开展业务,在质量和技术领先地位方面享有盛誉,并拥有强大的合作伙伴生态系统,可帮助支持、维护和促进互联世界的业务增长。