Skip to main content
globe
地区和语言 {{(header.eyebrow.langSelector.label != '') ? header.eyebrow.langSelector.label : getTranslation('panduit.localeselect.chooselanguage')}}
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
Panduit Launches 400G Next Generation CS® Connector to Optimize Data Center Fiber to Rack Density

 

TINLEY PARK, Ill. — (February 2, 2021) — As bandwidth speeds continue to increase, 200G/400G applications are becoming commonplace in high performance data center environments, requiring enhanced capabilities at the rack level. Panduit has launched the CS® Connector, a high-density fiber connector solution that optimizes the data center for next generation applications. Its compact size enables breakout mode options and improves compute density for 25G-400G deployments. The CS Connector is available for unitary Singlemode and Multimode fiber options.

Complex applications including AI and Machine Learning are driving the need for higher data density in the rack and increased data per port. CS connectors offer an elegant solution by enabling two duplex CS patch cords (four fibers) to fit in QSFP-DD and OSFP transceivers. This doubles the number of fibers compared to LC patch cords and enables 200G per port today and 400G in the future. Panduit’s CS Fiber Patch Cords and Cassettes also provide 40% greater port density per rack unit (RU) than LC Connectors when used in Panduit’s HD Flex™ Fiber Cabling system.

The Push-Pull Connector and unitary cable design reduce congestion in pathways and allow easy access in high-density applications without disturbing adjacent circuits. This is important as CS Connector-based solutions can offer up to 216 connections per RU compared to only 144 connections using LC Connectors. The new small form factor CS Connectors allow for a reduced connectivity footprint which enables more efficient space utilization in hyperscale, multi-tenant and large data center environments.

Panduit is a founding member of the CS Consortium, which is a vendor neutral organization dedicated to educating end users and design consultants on the technical merits of the CS Fiber Connector solution.

关于 Panduit

自 1955 年以来,Panduit 的进取精神和解决问题的探索热情帮助许多公司在业务目标与市场成功之间搭建起了桥梁。Panduit 为从数据中心到电信机房、从台式机到工厂的各种企业级环境创建领先的物理、电气、网络基础设施和音视频解决方案。Panduit 总部位于美国伊利诺伊州廷利公园,在全球 112 个地区开展业务,在质量和技术领先地位方面享有盛誉,并拥有强大的合作伙伴生态系统,可帮助支持、维护和促进互联世界的业务增长。