What 29 Years of Short-Circuit Testing Taught Me About Cable Cleat Standards
In working with cable cleats for 29 years, I've introduced scores of innovative cable cleat designs, been deeply involved in their manufacture, and carried out thousands of short-circuit tests. I have seen awareness increase and adoption in the field grow, but nothing has done more to drive cleat implementation than technical standards. I've had a front-row seat as every major standard was being developed since the original BS EN 50368 and its successor, IEC 61914, and this article will shed some light on how they came about.
Cable Cleats Are in the Code
The NEC lays out the requirements for cable restraint without specifically mentioning cable cleats or explaining how to meet the requirement. This is why standards matter.
NEC 392.20 states, “Single conductor cables shall be securely bound in circuit groups to prevent excessive movement due to fault current forces.”
NEC 370.2 states, “Cable bus, an assembly of units including insulated conductors... This assembly is designed to carry fault current and to withstand the magnetic forces of such current.”
NEC 110.36 states, “Insulators, together with their conductor attachments, where used as supports for single-conductor cables, shall all be capable of safely withstanding the maximum magnetic forces that would prevail if two or more conductors of a circuit were subjected to short-circuit current.”
How Cable Cleat Standards Evolved
I sat on the original CENELEC working group starting in 1999. We first published a British BS EN standard in 2003, and we turned that BS EN into an IEC standard in 2009. Much of the technology within that standard comes from European utility requirements, including two successive short circuits due to pole-top reclosers and the type of cable used.
Once I joined Panduit, we realized there was a need for North American standards so contractors, engineers, and consultants could look at the requirements in the code and know how to meet them. We started different working groups, and the first organization we approached was CSA, which was very open to forming a working group for cable cleats.
Our task force started with the IEC standard and then discussed what needed to change to make it more regionally applicable for Canada and the rest of North America. We realized right away that we needed to consider highly flexible DLO cables and multicore cables with three or four conductors in the same jacket.
The auto-closers that operate at the top of utility poles in the United States and Canada can operate twice, so the system can experience three short circuits in a row instead of two, as is common in Europe. Over three years, we wrote these differences into the CSA standard, which was published in 2023.
We then approached NEMA, the National Electrical Manufacturers Association, to determine whether it wanted to develop a bulletin on cable cleats. NEMA was interested, and after committee review, we aligned on adopting the same requirements as CSA. The NEMA standards were published in 2024. When we test in accordance with CSA standards, we can apply the results to NEMA.
During this time, I have also been chairing the cable cleats working group for UL. After 18 months of collaboration, UL formally adopted cable cleats and published its DWMU/7 standard at the end of 2025. Panduit is the first company globally to attempt to obtain that listing. To date, we have conducted 200 live short-circuit tests witnessed by UL representatives, and we expect at least 90% of our cable cleat line to be UL Listed soon.
Will the New Standards Affect the Code?
When I started at Panduit, most installers used plastic cable ties to manage cables. They are quick and inexpensive, and a long cable run can look straight and neat. But when cables experience a short circuit, cable ties provide no meaningful resistance to the electromagnetic forces and can break apart.
As members of NEMA, we can submit recommendations to the NEC code-making process. The current language leaves room for interpretation, and because this is a safety issue, we have formally raised the topic of cable cleats with the NEC through NEMA field engineers under IEEE.
In the next revision of the NEC, our hope is that the code will not only say that cables must be restrained, but also explain how.
See what happens without proper restraint
What's in NEMA BI 50018-2024?
There are two primary regional differences between IEC and NEMA/CSA requirements: cable types and the number of short-circuit events.
NEMA requires testing on three cable types: approved Class B, flexible DLO, and multicore. A three-foot section of Class 2 500 kcmil copper is difficult to bend, whereas DLO can be bent to 90 degrees more easily. Added flexibility can change test results, but not always as expected. In some configurations, the added stiffness of Class 2 cable transfers more force to the cleat; in others, it transfers less.
See cable cleats in action during a short circuit.
The number of short-circuit events a cleat must withstand is a significant difference. NEMA requires three successive events. The cables must then be sprayed with water for at least two minutes before a withstand-voltage test of at least one minute confirms whether damage has occurred.
Every Panduit cable cleat has passed either two or three short-circuit events plus a water-spray and withstand test. We are the first manufacturer to meet the new standards for the top-selling 80% of our cleat offering.
How Are the New UL Standards Different?
The UL standards differ in two primary ways: testing follows the UL process, and the power source must be calibrated.
UL requires that all tests be witnessed by a UL representative, including all the set-up, installation, bolt torquing, etc. This time-consuming process ensures that all manufacturers are following the proper protocol, which gives UL the confidence to List the products.
The most significant change in the UL standards is voltage verification. Before a test is conducted, the lab must check the power source and calibrate it to the correct range. Previously, it was possible for a manufacturer to fudge the power levels slightly to achieve a successful test result. UL is making sure that everyone starts on a level playing field, which we fully support.
What's Next for Cable Cleats?
I expect cable cleat adoption to continue at a rapid pace. The need for proper cable restraint is real, and the benefits are undeniable when a short-circuit occurs. I’ve seen several cases where properly specified cleats prevented significant damage, and others where plastic cable ties failed and led to a cascading failure with significant costs.
We expect cable cleats to be explicitly mentioned in the next revision of the NEC code. This will bring much needed clarity and ensure that new factories, data centers, and energy infrastructure are being built to the minimum safety standards. At Panduit, we are continuing to innovate and push for cleat adoption globally.
Looking for the proper cable cleat for your next project? Use our online Cable Cleat kAlculator for recommendations based on four data points, or Contact Us.
For more information about Cable Cleats, visit panduit.com/cable-cleats.
- Liquid Cooling for Data Centers - Future-Ready AI & HPC Infrastructure
- What 29 Years of Short-Circuit Testing Taught Me About Cable Cleat Standards
- 3 Hidden Pathway Risks and How to Prevent Them with Cable Management
- Fault Managed Power: Answering the Questions Everyone is Asking
- The Product Nobody Thinks About—Until a Short Circuit Hits
- AI-Ready Infrastructure
- Smart Buildings and Enterprise Networks
- Future-Ready Data Centers
- Best Practices and Education
- Sustainability
- Industrial Transformation
- Sustainability and Infrastructure Efficiency
- Energy
- Best Practices and Education
- Digital Transformation
- Workforce Transformation
- Electrification