Skip to main content
globe
Region & Language {{(header.eyebrow.langSelector.label != '') ? header.eyebrow.langSelector.label : getTranslation('panduit.localeselect.chooselanguage')}}
Product Country of Use
{{getCountryTranslation()}}
{{ distyMobilePopUpData.title }}
{{ distyMobilePopUpData.primarybody }}
{{ distyMobilePopUpData.secondarybody }}
{{header.eyebrow.bom.label}}
{{addedBomQuantity}} {{addedBomName}} Added
{{totalQuantityInBom}} item(s) View List >>

Awards & Achievements

Industry recognition for innovation and customer collaboration.

Two images of the Panduit EL2P Power Distribution Unit in black with gray and turquoise accents

2026 Data Centre Solutions Awards Power Distribution Unit of the Year - Runner Up

Panduit EL2P (Elevate to Power) iPDU

Panduit was recognized for its EL2P iPDU which integrates advanced metering (±0.5%), robust cybersecurity, flexible outlet configurations, and comprehensive environmental sensing—key capabilities for hyperscale, enterprise, and colocation facilities.

Product Details
DCS Award Article

PXE MP550 mobile printer -light gray and black with touchscreen with the word Panduit

2026 EC&M Product of the Year-Labelers & Printers Category

MP550 PXE Series Mobile Printer

Panduit's MP550 PXE series mobile printer received accolades for its 300 dpi high-resolution printing which supports both die-cut and continuous labels up to 2 in. wide, as well as automatic full and half-cut capabilities with user-replaceable cutter units. The built-in Wi-Fi connectivity printer also features a 4.3-in. color LCD touchscreen and integrated QWERTY keyboard which reduces labeling time and streamlines workflows.

Product Details
EC&M Award Article

Two components of the Panduit FMPS shown (black with bright blue accents)

2025 ISE (ICT Solutions & Education) Network Innovator's Award - Gold Honoree

Fault Managed Power System (FMPS)

ISE recognized the Panduit's UL-Certified FMPS for revolutionizing broadband deployment by delivering safe, efficient, and cost-effective power over long distances. FMPS is able to actively monitor for 7 types of faults and stop power transmission within 2 milliseconds if any fault is detected, transmit 600 watts of power of a single 16AWG copper pair, and reach a maximum distance of 2 kilometers.

Product Details
ISE Network Innovator's Award Article

Young Female and Male at Panduit WorldSkills booth learning to change a cable fiber

2025 Asia Responsible Enterprise Award 

APAC Skills Change Lives Campaign

Panduit received the 2025 AREA in recognition of its APAC Skills Change Lives Campaign. The award highlights the campaign's contributions to bridging the skills gap and advancing youth empowerment in the Asia-Pacific region.

AREA Award Article
Campaign Details

Two images of the Panduit EL2P Power Distribution Unit in black with gray and turquoise accents

2025 Cabling Innovators Award - Platinum Level 

EL2P Intelligent Power Distribution Unit 

The Platinum Award for Panduit EL2P iPDU delivers visibility through brightly labeled outlets and a user-centric interface, speeds installation through innovative physical design, and simplifies updates through automated provisioning and secure firmware syncs.

Product Details
Cabling Innovators Award Article

Laptop on a table with a person's hands ready to use and book icons above the laptop

2025 Cabling Innovators Award - Gold Level

Rockford Public School System and Miller Electric Company Application Case Studies 

CI&M awarded Panduit a Gold award for two of their application case studies-Rockford Public School system and Miller Electric Company in which Panduit’s technologies were implemented. 

Rockford Public Schools Case Study
Miller Electric Company Case Study

Panduit black G6 PDU

2025 Data Centre Solutions Technology Award

G6 Power Distribution Unit

The G6 PDU received the DCS Technology Award for its low-profile design that saves rack space while increasing airflow. It also provides 128 times the memory of a G5, while offering industry-leading outlet density and the ability to daisy chain up to 32 PDUs.

Read the Press Release
DCS Award Article

2023 Occupational Health & Safety Industrial Hygiene Award - Facility Safety

VeriSafe™ 2.0 Absence of Voltage Testers

OH&S recognized the VeriSafe 2.0 Absence of Voltage Tester for its innovative way to test for the absence of voltage safely, reliably, and efficiently with exposure to electrical hazards.

Product Details
Read the Press Release

2022 Best in Class Employer

Panduit Recognized by Gallagher

Panduit was one of the 4,000 participating organizations in the 2022 Benefits Strategy & Benchmarking Survey, which forms part of Gallagher’s influential U.S. Workforce Trends Report Series.

Join Our Team

2022 Cabling Innovators Award - Platinum Level

GIGA School Concept Application

The winning case study application highlighted how Japan’s Kawachinagano City Board of Education selected Panduit products for all the wiring materials and parts to be installed for their GIGA schools including its Advanced Vari-MaTriX Category 6A cables, field term plugs, and patch cords.

Read the Case Study
Read the Press Release

2022 Cabling Innovators Award - Platinum Level

RapidID™ Network Mapping System

CI&M recognized the innovative RapidID™ Network Mapping System as a practical alternative to traditional manual approaches to the cable documentation process with a solution using patch cords pre-labeled with unique barcodes and a Bluetooth®-enabled handheld scanner to automate labeling, tracing, and troubleshooting.

Product Details
Read the Press Release

2022 Cabling Innovators Award - Gold Level

FieldCord™ Connector

The FieldCord™ Connector was recognized by CI&M for being designed specifically to connect devices such as cameras and access points that have small openings for cords or plugs.

Product Details
Read the Press Release

2022 Cabling Innovators Award - Gold Level

FlexCore™ Optical Distribution Frame

The FlexCore™ ODF system was recognized for enabling a consolidated patch cord length to be used between a single, double, or quad frame arrangement, freeing up capital that is tied up in holding inventory, and ensuring the customer always has the right parts on hand.

Product Details
Read the Press Release

2022 Cabling Innovators Award - Gold Level

PanMPO™ Fiber Connector

The enhanced PanMPO™ Fiber Connector was recognized by CI&M for its innovative push-pull boot that allows for easy installation and removal, as well as it has the ability to change gender and polarity without additional tools. 

Watch the Video
Read the Press Release

2022 Cabling Innovators Award - Gold Level

Uninterruptible Power Supply

The Uninterruptible Power Supply was recognized by CI&M for its delivery of highly efficient and reliable power protection and backup power for IT equipment by providing excellent electrical performance, intelligent battery management, enhanced intelligent monitoring, secure network functions, and a long lifespan for lithium units.

Read the Press Release

2022 Cabling Innovators Award - Silver Level

Wire Basket Overhead Cable Tray Routing System

The Wire Basket Overhead Cable Tray Routing System was recognized for contributing to effective space utilization, reduced installation time, and network performance by providing a greater strength-to-weight ratio than other wire baskets as well as the design of its wire mesh grid pattern which allows greater amounts of cables and QuickNet Cassettes to pass grid openings without additional cutting.

Product Details
Read the Press Release

2021 Cabling Innovators Award - Platinum Level

Single Pair Ethernet

Single Pair Ethernet, receiving platinum honoree, is a seamless single protocol network from application edge to the cloud. SPE simplifies network design and operation, eliminating the support and translation of legacy network protocols used in OT networks.

Learn More

2021 Cabling Innovators Award - Gold Level

PanZone® TrueEdge™ Wall Mount Enclosure

The PanZone® TrueEdge™ Wall Mount Enclosure, receiving gold honoree, minimizes network infrastructure investment by providing a solution to eliminate a rack or cabinet.

Watch Video
View Solution

2021 Cabling Innovators Award - Gold Level

FlexFusion™ Cabinet

The FlexFusion™ Cabinet, receiving gold honoree, offers a unique universal platform for all types of data centers and servicing needs including Hyperscale, Edge, and Colocation. The cabinet is built with a best-in-class weight load of 3,500 lbs., doors with a maximum airflow of 80%, and custom configurations to meet network needs.

Learn More
View Solution

2021 Cabling Innovators Award - Silver Level

Adjustable Depth 4-Post Racks

Adjustable Depth 4-Post Racks, receiving silver honoree, combine the stability of a cabinet with the accessibility of an open rack to provide users with maximum flexibility when designing the network layout.

View Selection Guide
View Solution

2021 Cabling Innovators Award - Silver Level

TX6A™ FieldCord™ Connectors

The TX6A™ FieldCord™ Connectors, receiving silver honoree, enable connection to devices in the most confined cable routing paths and has the capability to be re-terminated up to 20 times with no additional parts.

Watch Video
View Solution

2020 Cabling Innovators Award - Gold Level

HD Fusion Wall Mount Enclosure

The HD Fusion Wall Mount Enclosure was recognized by CI&M as a fiber cabling solution that houses, organizes, manages, and protects cable-to-cable fusion splice connections and comes in two different sizes to splice up to 3,456 fibers or 6,912 fibers. 

Product Details
Read the Press Release

2020 Cabling Innovators Award - Gold Level                                                       

HD Flex™ Zone Raised Floor Enclosure

CI&M recognized the HD Flex™ Zone Raised Floor Enclosure as a structured cabling solution that saves valuable real estate in the data center by allowing cable terminations below raised floors, helping to relieve rack and cabinet congestion. 

Product Details
Read the Press Release

2020 Cabling Innovators Award - Platinum Level

UC Davis Medical Center

The CI&M Platinum winning case study highlights the 14-year partnership between UC Davis Medical Center, Panduit, and General Cable. The medical center is supported by four data centers (one on-premises and three colocation facilities), and more than 250 telecommunications rooms. The campus has more than 70,000 cable drops, equating to more than 140,000 Panduit connectors, and more than 12 million feet (more than 2,300 miles) of cable.

Read the Case Study
Read the Press Release

2020 Cabling Innovators Award - Gold Level

PatchRunner™ 2 Cable Management System

CI&M recognized the PatchRunner™ 2 Cable Management System as a cabling solution that manages growing cable densities, larger network equipment, and increasing energy usage.

Product Details
Read the Press Release