Comunicado de prensa
Panduit Honored in 2021 Cabling Installation & Maintenance Innovators Award
TINLEY PARK, Ill. — (August 31, 2021) — Panduit, a global leader in innovative electrical and network infrastructure solutions, was recognized today with five Cabling Innovators Awards in the 2021 competition. Cabling Installation & Maintenance bestows the Innovators Awards annually to the best products and projects in the industry.
Panduit received five awards in total, including a Platinum honor for Single Pair Ethernet (SPE) solution, a seamless single protocol network from application edge to the cloud. SPE simplifies network design and operation, eliminating the support and translation of legacy network protocols used in OT networks.
“With the emergence of Single Pair Ethernet technology built for OT applications, we expect to see accelerating growth in wired Ethernet in place of fieldbus and analog communications,” states Mike Vermeer, Engineering Development Strategy Manager. “Panduit is grateful to be recognized for our efforts to bring this technology to market, and we are excited for the possibilities this brings to intelligent buildings, smart factories and Industry 4.0.”
Panduit also received two Gold awards and two Silver awards:
- FlexFusion™ Cabinet (Gold Honoree) - Offers a unique universal platform for all types of data centers and servicing needs including Hyperscale, Edge and Colocation. The cabinet is built with best-in-class weight load of 3,500 lbs., doors with maximum air flow of 80%, and custom configurations to meet network needs.
- PanZone® TrueEdge™ Wall Mount Enclosure (Gold Honoree) - With 0 RU vertical patching, the enclosure’s mounting method minimizes network infrastructure investment by providing a solution to eliminate a rack or cabinet.
- TX6A™ FieldCord™ Connectors (Silver Honoree) - Enable connection to devices in the most confined cable routing paths and has the capability to be re-terminated up to 20 times with no additional parts.
- Adjustable Depth 4-Post Racks (Silver Honoree) - Combines the stability of a cabinet with the accessibility of an open rack to provide users with maximum flexibility when designing the network layout.
“Helping customers gain competitive advantage and ensuring their utmost satisfaction is a core focus for Panduit. Taking the time to understand each customer’s unique infrastructure needs has helped us to innovate new products that will allow them to grow in this ever-evolving, modernized world,” states Marc Naese, Senior Vice President of Network Infrastructure. “Receiving five CI&M Innovators Awards is an honor and we are incredibly thankful for the recognition.”
For more information, click here to visit Cabling Installation & Maintenance’s website.
Acerca de Panduit
Desde 1955, la cultura de Panduit de la curiosidad y pasión por la resolución de problemas han permitido conexiones más significativas entre las metas de negocio de las empresas y su éxito en el mercado. Panduit crea soluciones avanzadas de infraestructura física, eléctrica y de red para entornos empresariales, desde el centro de datos hasta el piso de manufactura, pasando por el escritorio y cuarto de telecomunicaciones. Con sede en Tinley Park, IL y operando en 112 países, la probada reputación de Panduit de liderazgo en calidad y tecnología, junto con un sólido ecosistema de socios, nos permiten apoyar, mantener e impulsar el crecimiento del negocio en un mundo conectado.
Contacto de prensa
Global
Dawn Leach
Manager Global Brand
Tel. 708-532-1800 ext. 81316
Dawn.Leach@panduit.com
LATAM
Miranda Alexandra Sánchez
Marketing Communication Specialist
Tel. 800 360 86 00
MirandaAlexandra.Sanchez@panduit.com
Monica Lechuga
Marketing Communications Manager
Tel. 800 360 86 00
monica.lechuga@panduit.com