Skip to main content
globe
Región e idioma {{(header.eyebrow.langSelector.label != '') ? header.eyebrow.langSelector.label : getTranslation('panduit.localeselect.chooselanguage')}}
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
Comunicado de prensa

Panduit Launches 400G Next Generation CS® Connector to Optimize Data Center Fiber to Rack Density

 

TINLEY PARK, Ill. — (February 2, 2021) — As bandwidth speeds continue to increase, 200G/400G applications are becoming commonplace in high performance data center environments, requiring enhanced capabilities at the rack level. Panduit has launched the CS® Connector, a high-density fiber connector solution that optimizes the data center for next generation applications. Its compact size enables breakout mode options and improves compute density for 25G-400G deployments. The CS Connector is available for unitary Singlemode and Multimode fiber options.

Complex applications including AI and Machine Learning are driving the need for higher data density in the rack and increased data per port. CS connectors offer an elegant solution by enabling two duplex CS patch cords (four fibers) to fit in QSFP-DD and OSFP transceivers. This doubles the number of fibers compared to LC patch cords and enables 200G per port today and 400G in the future. Panduit’s CS Fiber Patch Cords and Cassettes also provide 40% greater port density per rack unit (RU) than LC Connectors when used in Panduit’s HD Flex™ Fiber Cabling system.

The Push-Pull Connector and unitary cable design reduce congestion in pathways and allow easy access in high-density applications without disturbing adjacent circuits. This is important as CS Connector-based solutions can offer up to 216 connections per RU compared to only 144 connections using LC Connectors. The new small form factor CS Connectors allow for a reduced connectivity footprint which enables more efficient space utilization in hyperscale, multi-tenant and large data center environments.

Panduit is a founding member of the CS Consortium, which is a vendor neutral organization dedicated to educating end users and design consultants on the technical merits of the CS Fiber Connector solution.

Acerca de Panduit

Desde 1955, la cultura de Panduit de la curiosidad y pasión por la resolución de problemas han permitido conexiones más significativas entre las metas de negocio de las empresas y su éxito en el mercado. Panduit crea soluciones avanzadas de infraestructura física, eléctrica y de red para entornos empresariales, desde el centro de datos hasta el piso de manufactura, pasando por el escritorio y cuarto de telecomunicaciones. Con sede en Tinley Park, IL y operando en 112 países, la probada reputación de Panduit de liderazgo en calidad y tecnología, junto con un sólido ecosistema de socios, nos permiten apoyar, mantener e impulsar el crecimiento del negocio en un mundo conectado.

Contacto de prensa

Global

Dawn Leach
Manager Global Brand
Tel. 708-532-1800 ext. 81316
Dawn.Leach@panduit.com

LATAM

Miranda Alexandra Sánchez
Marketing Communication Specialist
Tel. 800 360 86 00
MirandaAlexandra.Sanchez@panduit.com

Monica Lechuga
Marketing Communications Manager
Tel. 800 360 86 00
monica.lechuga@panduit.com