Comunicado de prensa
Panduit Collaborates with Cisco to Drive Data Center Sustainability
TINLEY PARK, Ill. — (August 16, 2023) — Panduit Corp., announces its collaboration to integrate its intelligent PDU (iPDU) with the Cisco Nexus Dashboard. This integration empowers data center managers with enhanced visibility into energy usage, carbon footprint, and cost across both on-premises and multi-cloud environments. Cisco announced the collaboration with Panduit at Cisco Live 2023 in Las Vegas.
“Together, Cisco and Panduit can help our joint customers build resilient, energy efficient, and high-performance data centers," stated Panduit Vice President of Data Center, Holly Garcia. "Our collaboration has grown beyond network infrastructure to the strategic area of power and sustainability. We have partnered with Cisco to streamline data from our intelligent PDU (iPDU) into Sustainability Insights on Cisco Nexus Dashboard. We are dedicated to driving greater visibility into sustainability with Cisco, enabling customers to monitor and forecast their future energy needs, costs, as well as carbon emissions through our integration with Nexus Dashboard.”
The urgent need for sustainability initiatives has evolved from a regulatory and compliance necessity to a critical business imperative. Gartner predicts that by 2027, 75% of organizations will have implemented a data center sustainability program. Rising energy and material costs, escalating power requirements, and impending regulations have intensified the urgency surrounding climate action. Technology vendors such as Cisco and Panduit play a pivotal role in providing solutions for data centers, which contribute to global greenhouse gas emissions. The integration of the Cisco Nexus Dashboard and Panduit iPDU will equip customers with the necessary data to help accelerate their sustainability roadmap, regardless of whether they are just beginning or are well along their journey to achieving net zero.
For more information, please visit www.panduit.com/panduitciscoalliance
About Cisco
Cisco (NASDAQ: CSCO) is the worldwide technology leader that securely connects everything to make anything possible. Our purpose is to power an inclusive future for all by helping our customers reimagine their applications, power hybrid work, secure their enterprise, transform their infrastructure, and meet their sustainability goals. Discover more on The Newsroom and follow us on Twitter at @Cisco.
Cisco and the Cisco logo are trademarks or registered trademarks of Cisco and/or its affiliates in the U.S. and other countries. A listing of Cisco's trademarks can be found at www.cisco.com/go/trademarks. Third-party trademarks mentioned are the property of their respective owners. The use of the word partner does not imply a partnership relationship between Cisco and any other company.
Acerca de Panduit
Desde 1955, la cultura de Panduit de la curiosidad y pasión por la resolución de problemas han permitido conexiones más significativas entre las metas de negocio de las empresas y su éxito en el mercado. Panduit crea soluciones avanzadas de infraestructura física, eléctrica y de red para entornos empresariales, desde el centro de datos hasta el piso de manufactura, pasando por el escritorio y cuarto de telecomunicaciones. Con sede en Tinley Park, IL y operando en 112 países, la probada reputación de Panduit de liderazgo en calidad y tecnología, junto con un sólido ecosistema de socios, nos permiten apoyar, mantener e impulsar el crecimiento del negocio en un mundo conectado.
Contacto de prensa
Global
Dawn Leach
Manager Global Brand
Tel. 708-532-1800 ext. 81316
Dawn.Leach@panduit.com
LATAM
Miranda Alexandra Sánchez
Marketing Communication Specialist
Tel. 800 360 86 00
MirandaAlexandra.Sanchez@panduit.com
Monica Lechuga
Marketing Communications Manager
Tel. 800 360 86 00
monica.lechuga@panduit.com