Skip to main content
globe
地区和语言 {{(header.eyebrow.langSelector.label != '') ? header.eyebrow.langSelector.label : getTranslation('panduit.localeselect.chooselanguage')}}
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
PDU Mass Deployment Made Simple: Introducing uPDU for Global Data Centers

Electricity is one of the essential utilities in a computing environment. And while the physics of electricity (illuminated by greats like Faraday, Edison, and Tesla) is constant, there’s considerable diversity in how power is transmitted and distributed worldwide. 

Take, for example, the deployment of 415 Volt power in North American data centers. In 2023, this isn’t particularly newsworthy. Fifteen years ago, it was novel. Around that time, big data center operators in North America proposed this “international” voltage as an avenue to greater data center efficiency—smaller transformers, fewer losses, and better utilization of power supplies.

Electrical diversity has conditioned us to look at electricity through regional silos. Still today, the prevailing practice is to segment power products according to regional electrical standards and regional conformance bodies like UL & CE. Therefore, any global enterprise likely has unique PDUs for each country/region in which they operate. This leaves a supply chain organization with more to manage—inventory levels, BOMs, configurations—and more opportunity for error.

The Panduit Universal PDU (uPDU) offers an avenue to address PDU deployment challenges. 

As soon as a cord/plug is hardwired to a PDU, it becomes regional—the opposite of ‘universal’ and the cause of the supply chain complexities mentioned above. The uPDU is deliberately sold absent a cord and plug and instead offers (12) potential choices called facility side cables.

updu-blog-side-image - 1

Consumers will choose the appropriate cable depending on the installation location and capacity required. The two components—PDU and cord—then mate on-site with no required tools. 

Facility Side Cordsets 

Part Number                                              Description                                                                                  Drop Down Menu in Web GUIApparent Power (kVA)       Input Voltage (V)Input Phase      
UPDUCRD1UPDU to IEC 60309 3P+N+E 6h 32A (IP44), CORD SET, 3M (10FT)32A3WYE"17.3 (NAM)
22.0 (EMEA)"
4153
UPDUCRD2UPDU to IEC 60309 2P+E 6h 60A (IP44), CORD SET, 3M (10FT)"60A1L-L (NAM) 60A1L-N (EMEA)"102081
UPDUCRD3UPDU to IEC 60309 3P+E 9h 60A (IP44), CORD SET, 3M (10FT)60A3DLT17.32083
UPDUCRD4UPDU to CS8365C 50A, CORD SET, 3M (10FT)50A3DLT14.42083
UPDUCRD5UPDU to IEC 60309 3P+N+E 6h 63A (IP44), CORD SET, 3M (10FT)"60A3WYE (NAM) 63A3WYE (EMEA)"

"23.0 (NAM)

27.6 (EMEA) BREAKER LIMITED"

4153
UPDUCRD6UPDU to IEC 60309 3P+N+E 6h 20A (IP44), CORD SET, 3M (10FT)"20A3WYE (NAM) 16A3WYE (EMEA)"

"11.5 (NAM)

11.0 (EMEA)"

4153
UPDUCRD7UPDU to L6-30P 30A, CORD SET, 3M (10FT)30A1L-L52081
UPDUCRD8UPDU to IEC 60309 2P+E 6h 20A (IP44), CORD SET, 3M (10FT)"20A1L-L (NAM) 16A1L-N (EMEA)"

"3.3 (NAM)

3.6 (EMEA)"

2401
UPDUCRD9UPDU to IEC 60309 2P+E 6h 32A (IP44), CORD SET, 3M (10FT)"30A1L-L (NAM) 32A1L-N (EMEA)"

"5.0 (NAM)

7.4 (EMEA)"

2401
UPDUCRD10UPDU to L21-30P 30A, CORD SET, 3M (10FT)30A3WYE8.62083
UPDUCRD11UPDU to L15-30P 30A, CORD SET, 3M (10FT)30A3DLT8.62083
UPDUCRD12UPDU to CS8265C 50A, CORD SET, 3M (10FT)50A1L-L8.32081

* User must select the appropriate drop down from WebGUI menu to achieve stated power metering accuracy.

For a full listing of part numbers including related products, please visit here

The uPDU capacity ranges from 3.3kVA to 27.6 kVA. The internal wiring is sized for the maximum possible current, making it safe to operate at all levels.

 

Use Cases   

Consistency: A user can deploy the same PDU everywhere and stock only the cords needed at each location.

Compliance: Universally compliant PDUs that meet international standards for PDUs[FM3] [RL4]

  • USA & Canada: UL/EN/IEC 62368 PDU
  • Europe - CE/UKCA Approved
  • Australia - RCM Approved
  • Brazil: Approved
  • Chile: Approved
  • Peru: Approved
  • United Arab Emirates (UAE): Approved
  • India: Approved
  • China: Approved
  • Hong Kong: Approved
  • Singapore: Approved

 

Adaptability: A recently acquired company faced changing rack power requirements as it had to move its IT gear into the data center of its new owner—one with a completely different power infrastructure. All the existing PDUs had to be scrapped for new models to accommodate these changes. In the same scenario, the uPDU offered a versatile solution, as it could be repurposed in the new environment simply by swapping the facility side cables, thus addressing the altered rack power demands efficiently.

Sustainability: Sustainability is more important than ever. The previous example speaks to it. Traditional rack PDUs may contribute to e-waste when replaced, and new product packaging and transportation can have environmental impacts. Not only do uPDUs keep PDUs from getting scrapped, but data centers save on the packaging and transportation that new products would require.

Summary

The uPDU is a departure from a conventional PDU—not applicable to all consumers but a difference maker for those who operate globally or who have diverse electrical systems to work within.

To learn more about Panduit Critical Power Solutions offering, please visit here.

分享此帖
作者。 Justin Blumling

Justin Blumling is a Technical Sales Engineer at Panduit. He has over twenty years of technical and commercial experience within data centers, including electrical, mechanical, cabinets, and DCIM. He supports Panduit’s Intelligent Infrastructure offering, comprised of rack PDUs, UPS, DCIM software, and intelligent sensors. He holds a Master of Business Administration (MBA) degree and is a US Department of Energy (DOE) certified Data Center Energy Practitioner – Specialist.