The Key to Predictable Fiber Deployment? Address the Bottlenecks
In our previous blog, “Building a Smart Framework for Outside Plant Fiber Deployment", we established a three-stage framework for outside plant design decisions. Now we tackle the challenge that keeps project managers up at night: permitting and make-ready delays – the single largest recurring bottleneck adding delay, rework, and unplanned costs to fiber deployments.
While permitting challenges can’t be eliminated, they can be anticipated and built into predictable workflows.
Understanding the Fiber Deployment Permitting and Make-Ready Bottleneck
The permitting and make-ready process encompasses several complex, interconnected requirements:
- Right-of-way approvals and traffic control plans must be secured
- Stormwater best management practices need documentation
- Environmental reviews can't be skipped
- Utility coordination becomes critical, involving pole loading clearances, make-ready windows, and third-party attachment or joint use applications
Special corridors add another layer of complexity:
- Railroad and highway crossings require separate permitting, insurance, and flagging
- Call-before-you-dig – or 811 services – requires careful coordination around advance notice periods and allowable work windows
Why Permitting Becomes a Bottleneck
Several factors consistently create delays, including late discovery of conflicts, jurisdictional variables from county to county and state to state, and piecemeal handoffs and submittals. These issues routinely lead to week-long delays.
These aren't mysterious problems – they are predictable challenges that can be addressed through better planning and process design.
Strategies to Expedite Permitting
Several practical approaches can significantly reduce permitting delays:
- Develop Permit-Ready Templates: Create standardized packages that include pre-approved traffic control drawings, standard plan sheets, stormwater management practice notes, environmental worksheets, and crossing packages. Standardization speeds review approval.
- Pursue Batch Submittals: Group applications by corridor or zone, creating one reviewer packet for many locations to help streamline reviews.
- Front-Load Conflict Discovery: Find conflicts early using subsurface utility engineering and pole stress analysis before finalizing designs or submitting permits. This "truthing" process is especially critical in corridors with dense utilities or where records are known to be inaccurate. The investment in early verification prevents expensive rework later.
- Draft Schedules Around 811 Rules: Build your construction schedule around state-specific rules for advance notice, valid marking periods, and allowable work windows. Stagger ticket requests to maintain a rolling start rather than creating bottlenecks.
- Submit Complete Packages: Submit full packages - traffic control drawings, railway and highway crossing packages, environmental clearances, and acceptance checklists – to reduce information requests and expedite approvals.
These approaches ensure repeatability across projects and crews and allow you to scale successfully.
Matching Architecture to Field Hazards
Beyond permitting challenges, another critical decision at this stage involves matching your architecture choices to specific hazards you'll encounter in the field. Different environments demand different approaches.
A useful framework maps architecture choices against common hazards using a simple traffic-light system: green indicates recommended approaches, yellow means the approach can work with appropriate safeguards, and red means you should avoid that option.
- Water and Flood Risks: For areas prone to flooding, keep transport underground in conduit while placing access points in above-grade pedestals. This keeps your backbone sealed and splices out of standing water. This is the green default to protect critical infrastructure while maintaining serviceability.
- Freeze and Ice: When freeze or ice are the primary concern, the green choice is underground transport with above-grade access for serviceability. Aerial solutions are yellow: they can work with appropriate safeguards, but they require more active management.
- Wind and Storm Debris: In areas where wind and storm debris are significant risks, aerial infrastructure becomes problematic. The green approach here is underground for both transport and access, eliminating exposure to wind-driven damage.
- Difficult Soil or Rock Conditions: When soil conditions are challenging or you're dealing with extensive rock, aerial transport becomes the default green choice, with selective use of horizontal directional drilling at necessary crossings. Access can be above-grade or vault-based depending on other site factors. This approach minimizes expensive excavation while maintaining system integrity.
- Third-Party Traffic and Strike Risk: In areas prone to third-party strikes, the green approach requires underground transport in conduit, with access in a visible setback located away from traffic lanes where vehicle strikes are most likely. Visibility helps contractors and maintenance crews, while setbacks provide physical protection.
- Fire Risk: When controlled burning or wildfires are the risk, the default green approach is underground transport in conduit to protect the backbone, with above-grade access points allowing for easy expansion and updates without disturbing sealed underground infrastructure.
Pick the green default approach for each hazard you face. Use yellow options only when you can implement explicit safeguards and document them in your standards. Avoid red approaches unless extraordinary circumstances require them. In those cases, you’ll want to document the variance, identify mitigation measures, escalate for sign-off, and update your as-built documentation and inspection checklists.
Building Predictability into Your Process
The permitting bottleneck doesn't have to be unpredictable. Incorporating these strategies into your three-stage framework, transforms permitting from a mysterious delay into a manageable process with known timelines.
Similarly, matching architecture to hazards provides logical framework that helps you make consistent decisions across different crews and different geographic areas. When everyone understands the reasoning behind architecture choices, execution improves and quality becomes more consistent.
In Part 3 of this blog series, we'll explore deployment playbooks for specific hazards and discuss how building the right partner ecosystem enables you to successfully execute these strategies at scale. In the meantime, learn more about designing projects in our Fiber Broadband Association on-demand webinar: Mastering OSP Design Decisions: A Practical Guide to Risk, Standards, and Smart Deployment.